Cancel
Showing results for 
Search instead for 
Did you mean: 

Simulation Utilizing Multiple Processors

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

Can Simulation utilize more than one processor?

Answer

If you uncheck 'Iterative Solver' in the Create Study UI, and then edit the corresponding .RCF (i.e. C:\Program Files\Solid Edge ST5\Simulation\Common\NXNastranRCFiles\SENASTRANStressTet.PCF)file and change to "parallel=4", every time the sparse solver runs it will use all four processors.