Cancel
Showing results for 
Search instead for 
Did you mean: 

Text Profile on Circle

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

Why can’t I get a text profile to place at the top of a circle?

Answer

If you place a text profile along a circle the text will always be aligned with the start/stop point of the circle. In order to have more control of the text profile position use an arc instead. The text profile will align with the arc midpoint, which can be controlled. The start/stop point of a circle cannot be controlled.

Contributors