Cancel
Showing results for 
Search instead for 
Did you mean: 

When no variables listed in the Variable Table

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

What can I do if there are no variables listed in the variable table, but they are supposed to?

Answer

Go to the Variable Table command, click on the Filter (funnel icon), ensure that entries in the Type list are highlighted (Dimensions, User Variables and PMI Dimensions), click 'Named by -> Both' option, click on 'Graphics in->File' option and click OK.

Contributors