Cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot view all of a long markup note

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

If I have a long markup (redline) note, only some of the note is visible.  Attempting to click on the scroll bar or another part of the note to see the rest of the note selects entities behind the note as if the note is not there.  In the attached image I clicked on the note at the "t" on the bottom line and it selects the ground from the model underneath.  We need a way to scroll through the rest of the note or resize the note to be able to read it all after the markup is saved.

Portal Markup Issue.png.

3 REPLIES 3

Re: Cannot view all of a long markup note

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hello,

 

Thanks for posting the query !! 

 

We can scroll or resize the note after the markup is saved.

All you need to do is,

  1. Select the markup.
  2. Goto 'Add Redline' command.
  3. Double click on redline textbox. You will observe that redline text object is selected.
  4. Once selected, you can scroll through the text or either change the textbox size.

Please refer the attached video for more details,

 

(view in My Videos)

 

Regards,

Sukrut Gadre.

Solid Edge Planning.

Re: Cannot view all of a long markup note

Solution Partner Creator Solution Partner Creator
Solution Partner Creator
Hi Sukrut,

Thanks for your reply. Are you are suggesting we cannot scroll or resize the note without entering the Add Redline command?

This seems a little counter-intuitive considering all I want to do is read what is in the note, not add a new Redline. Can the ability to either resize or scroll through the note (without entering the Add Redline command) be added to the Enhancement Requests list?

Best Regards,

TOM HARRIS | CAE APPLICATIONS ENGINEER
EDGE plm software pty ltd | Unit 16, 94-102 Keys Rd | P.O. Box 126 | Moorabbin Victoria 3189
Main: +61 3 9532 0700 | Fax: +61 3 9532 0788 | Mobile +61 432 270 535 | Support 1300 883 653
Webpage: www.edgeplm.com.auEmail: tom@edgeplm.com.au
P Please consider the environment before printing this e-mail.


Note:
This message is for the named person's use only. It may contain confidential, proprietary or legally privileged information. No confidentiality or privilege is waived or lost by any mistransmission. If you receive this message in error, please immediately delete it and all copies of it from your system, destroy any hard copies of it and notify the sender. You must not, directly or indirectly, use, disclose, distribute, print, or copy any part of this message if you are not the intended recipient. EDGE plm software and any of its subsidiaries each reserve the right to monitor all e-mail communications through its networks. Any views expressed in this message are those of the individual sender, except where the message states otherwise and the sender is authorized to state them to be the views of any such entity.

Re: Cannot view all of a long markup note

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hello,

 

Thanks for your response !

 

We can resize and read the Redline Note size without entering the command. But to scroll we must enter into the command.

 

Regards,

Sukrut Gadre

Solid Edge Planning.