Cancel
Showing results for 
Search instead for 
Did you mean: 

Share a project so that multiple users can upload files?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

 

I've shared a project with a colleague but the options I can give him are only "View" or "View and Download", so it means he can't upload a file of his own to the project. Which nullifies the shared work concept. Or am I missing something?

 

Best regards,

Carlos

1 REPLY 1
Highlighted

Re: Share a project so that multiple users can upload files?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Cadflow,

 

I believe Solid Edge Portal is [currently] only an "outward" sharing platform, so does NOT act like other cloud services such as Dropbox, OneDrive, GoogleDrive, etc.

 

Adding a "Collaborate" button, would be a welcome enhancement! Maybe @KeithCain could chime in?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000