Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Portal Known Issues

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Updated: May 7, 2018

 Solid Edge Portal

  • File upload does not support folders
  • Cannot enter more than one email address when sharing Projects

Viewer

  • Solid Edge 2019 files are not supported in the Viewer yet. They will be supported once Solid Edge 2019 is released.
  • It's recommended you use a keyboard and mouse when using the Edge browser with touch screen
  • Empty files cannot be displayed in the Viewer. At least one body must be present in the file for it to be viewable.
  • Limited support for viewing draft files.
    1. No preview picture on the carousel
3 REPLIES 3
Highlighted

Re: Solid Edge Portal Known Issues

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi I tried several times to upload a parasolid file (x_t exported from Solid Edge ST10 MP8) and it doesn't work whereas it is supposed to work according to the help page.

Re: Solid Edge Portal Known Issues

Siemens Genius Siemens Genius
Siemens Genius

Hi @aguitton116

 

I have been able to reproduce the problem.  This appears to be related to the Parasolid version used during translation.  I have logged a bug for this issue but as a temporary workaround it is possible to select Options during the save as to x_t and change the Parasolid version to 29.1.  Exporting with this version of Parasolid should correct the failing upload of your file(s).

 

Thanks,

Keith

 

Project Test Eng Adv

Mainstream Eng

Siemens Industry Sector

Siemens Product Lifecycle Management Software Inc

* Opinions expressed are my own.

Re: Solid Edge Portal Known Issues

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

OK thanks !