Cancel
Showing results for 
Search instead for 
Did you mean: 

Sync parts show PMI at assembly level

Genius
Genius

When using synchronous parts, the PMI dimensions show up at the assembly level (see attached).  I'd suggest that most users would see this as undesireable. An assembly of sync parts would be a mess.  

 

Assembly level PMI also shows up (as expected) but displays using the "model size PMI" .  In reality, if you use PMI in assemblies you most likely use the "pixel size" option which keeps PMI at a consistent size no mater the size of the assembly.  I'd suggest the same approach would be required for the Portal to make viewing PMI practical.

 

 

 

 

 

4 REPLIES 4

Re: Sync parts show PMI at assembly level

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Good spotting man.....I was wondering why some of my parts & assemblies had PMI dim's showing, and yup, those are my Sync parts.

 

With no way for the user to show/hide them, these become very annoying.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Sync parts show PMI at assembly level

Siemens Genius Siemens Genius
Siemens Genius

@RLR

@SeanCresswell

 

Hello,

 

The fact that PMI from parts are not shown in PathFinder, so that they can be turned off/on, is an issue that is being looked at.  I will post when this has been fixed and pushed to the Solid Edge Portal.

 

 

Thanks,

Keith

 

Project Test Eng Adv

Mainstream Eng

Siemens Industry Sector

Siemens Product Lifecycle Management Software Inc.

* Opinions expressed are my own.

Re: Sync parts show PMI at assembly level

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Great, thanks @KeithCain.......I did discover the context menu available to alter the displayed visibility, which helps.

 

Would be a good enhancement, if the user could multi-select items, to then apply the contextual option.

 

2018-02-26.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Highlighted

Re: Sync parts show PMI at assembly level

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Would be a good to add option hide all/show all PMI in the the contextual menu.