Academic code for ST6 Student Edition

Experimenter
Experimenter

Hello, I´ m Gastón, I from Argentina and I have installed SE ST6 Student Edition. However, I can´t find the academic code.  Where do I find it?. I can open the program normally but it´s imposible to use. Thank you very much!  

5 REPLIES

Re: Academic code for ST6 Student Edition

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Gaston!

 

You should be able to generate the academic license code here:

https://www.plm.automation.siemens.com/en/academic/resources/solid-edge/student-download.cfm

It should email it to you and give you intructions on how to set it up.

 

Also, is there any reason you're running ST6?

ST9 is the latest edition and it's still available absolutely free for students on the link above Smiley Happy

Kind Regards,
Jack Stark

Majenta PLM - Siemens Platinum Business Partner
http://majentaplm.com/

Re: Academic code for ST6 Student Edition

uk_dave 1st Gear
1st Gear

@JackStark FYI, ST6 is the last 32-bit version available

Re: Academic code for ST6 Student Edition

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

@uk_daveThanks! I think the ST9 academic codes should still work for ST6 as well

Kind Regards,
Jack Stark

Majenta PLM - Siemens Platinum Business Partner
http://majentaplm.com/

Re: Academic code for ST6 Student Edition

Experimenter
Experimenter

@JackStark Hi. I have installed the ST6 edition because my notebook does not support the ST9 version. It has a 64-bit Operating System but does not have a video card.For that reason I installed an older version, I study mechanical engineering and I need to use the program as soon as possible, even if it is not the last version. So, I have already registered and I have received the mail that is in the attached image, but I have not but I have not received any code yet. Smiley Sad 

 

Re: Academic code for ST6 Student Edition

KennyG 2nd Gear
2nd Gear

@Gaston, All versions of SE recommended a workstation class video card to support best performance and all graphic features, so ST6 or ST9 does not matter.  The advantage to ST6 is that it is available as 32 bit for those who are still running a 32 bit version of Windows.



Ken

Production: ST10 MP3
Testing: SE 2019