Another problems with installation SE !

N/A
Hi,

While i try to install SE (ST6) my CPU found an issue. It says: " The wizard was interrupted before Solid Edge ST6 could be completely installed. Your system has not been modified. To complete installation at another time, please run setup again".

Someone know what I shold do with this issue? I have win7 professional x64 and have service pack 2. I tried to find answer on google but I found nothing helpful. I hope someone here can help Smiley Happy

Thanks!
4 REPLIES

Re: Another problems with installation SE !

N/A
Same problem here! Tried everything I could find on the Internet and still the same problem! When trying to install ST3 and ST5 the same problem comes up! Please help Smiley Wink

Re: Another problems with installation SE !

Esteemed Contributor
Esteemed Contributor
Hi there,...try right clicking on the '.exe' file and choosing "Run As Administrator"....also, some anti virus apps can interfere with the install, try disabling temporarily.
-
Sent from my Samsung Galaxy S4 mobile, using Tapatalk 2.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Another problems with installation SE !

N/A
All that does not help, tried everything there is to find in other forum entries. No antivirus on, run as admin, service packs are installed, everything else closed on computer... everything! Please, there must be an answer!!! Smiley Very Happy

Re: Another problems with installation SE !

Siemens Phenom Siemens Phenom
Siemens Phenom
Disable UAC:
http://windows.microsoft.com/en-gb/windows-vista/turn-user-account-control-on-or-off
Temporarily disable anti-virus.
Using a file archiver/extraction program i.e. 7-zip
(http://www.7-zip.org/) manually extract the installer files from the
downloaded .exe file.
Right-click Run as Administrator on the setup.exe from your manually
extracted folder location.
Regards,
-Dave
On 14/11/2013 06:58, klaudias666@web.de wrote:
>
> All that does not help, tried everything there is to find in other forum
> entries. No antivirus on, run as admin, service packs are installed,
> everything else closed on computer... everything! Please, there must be
> an answer!!! Smiley Very Happy
>
>