Can Not Move Command

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

With This Short Video I Will Show You The Issue With The Move Command.

With This Video I Am Holding Down The Shift And Or CTRL...  I Am Only Able To Move Only One Item Not Multiples.

While The Other Commands Like The Rotate, Mirror, Scale Works Fine.

 

 

http://screencast.com/t/DIhUD3Mv3Z8B

 

Thank You 

GregoryLee

3 REPLIES

Re: Can Not Move Command

Siemens Legend Siemens Legend
Siemens Legend

Hi Gregory

 

It looks to me as if you might be doing this:

 

1.  Select the Move command.

2.  Select a circle.

3.  Press Shift.

4.  Select the second circle.

5. Click the "from" point.

6.  Click the "to" point.

 

Instead, you need to do this:

 

1.  Select the Move command.

2.  Press Shift.

3.  Select a circle.

4.  Press the second circle.

5. Click the "from" point.

6.  Click the "to" point.

 

You have to press Shift before you pick the first circle.  Otherwise the program thinks you are clicking the from point (doesn't recognize this as multi-select operation.)

 

You can also fence select multiple elements to move a group.

 

Hope this helps,

Melanie

Re: Can Not Move Command

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor
Melanie
This Issue Has Been Going Of A While Now.
These Videos Shows What The Commands Are Doing The Rotate, Mirror, Scale
Are Working Perfectly.
The First Video Shows The All Three Commands Working. POST: Keep An Eye On
The Cursors. The Magnifier Pointer Changes After Each Thread Is Selected.
The Second Video However, Shows The Move Command, Keep An Eye On The
Cursor... The Magnifier Pointer Changes After The First Thread Is Selected.
Also, The Cursor Changes To The Cross Cursor While Holding The Shift Key
Any Thoughts

Commands That Work:http://screencast.com/t/bGB9pre0tte

Move Command Not Working.
Also Will Show You The Rotate, Mirror, Scale
Work Fine.
I Do Hold Down The Shift.
http://screencast.com/t/bgy65gzOn7Y

Thank You
GregoryLee

Re: Can Not Move Command

Siemens Legend Siemens Legend
Siemens Legend

Hi Gregory,

 

I see the problem now.  It appears that this is a bug that has been fixed since ST8 was released.  For now, you can use fence select, or you can Shift select multiple elements and then select Move to relocate them.

 

Thanks

Melanie