Cant use solids!

Experimenter
Experimenter
I have the ST7 academic version and I need help. I recently applied the program and noticed that I did not have access to Extrude, Revolve, etc. This happened in school to but there was a way to turn it on. In school I used academic ST6. If anyone can help me enable the use of solids that would be greatly appreciated. Thank you.
1 REPLY

Re: Cant use solids!

Esteemed Contributor
Esteemed Contributor

Commands will be inactive if the conditions or environment is not right in which to use them.  For instance, if you are in Synchronous mode, those commands you mentioned will be inactive until you have created a sketch in which to use them on.



Ken

Production: ST10 MP3
Testing: SE 2019