Computer Issues

N/A
I went to get this computer to remove a virus. Getting it removed... Solid Edge is slower than ever. Is there a special computer tech trained to work with this type of drafting programs, tools ect. Ex, Within 1 hr. Must shut down no memory. Also, there isn't a redo arrow. Thoughts.

Thanks
Crousie
7 REPLIES

Re: Computer Issues

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom
I have yet to discover anyone who has ever gotten a virus on their
computer from a Solid Edge file or application (one of the reasons you
can't record custom macros.) For that reason, most users exempt the
Solid Edge file types and the edge.exe process from antivirus scanning.
This improves Solid Edge performance.
Otherwise, you will have to give us some hardware specs to see if you
have a computer tweaked for Solid Edge performance.
--Scott Wertel Phoenix Area Edger
On 5/1/2013 5:59 AM, Crouse@Concept-Dwgs.com wrote:
> I went to get this computer to remove a virus. Getting it removed...
> Solid Edge is slower than ever. Is there a special computer tech trained
> to work with this type of drafting programs, tools ect. Ex, Within 1 hr.
> Must shut down no memory. Also, there isn't a redo arrow. Thoughts.
>
> Thanks
> Crousie
>
>


____________________________________
--Scott Wertel, P.E.

Re: Computer Issues

N/A
Scott
Thanks for your reply, this is the specs for this computer.
http://screencast.com/t/onaCH2YK
http://screencast.com/t/eycHPq9M
http://screencast.com/t/AVxNEKrC31
I hope this info will shed some light.
Thanks
Crousie

Re: Computer Issues

KennyG 2nd Gear
2nd Gear
Are you stating that you took your computer to someone to have a virus removed and after you got it back, Solid Edge started behaving badly?


Ken

Production: ST10 MP3
Testing: SE 2019

Re: Computer Issues

N/A
After this computer came back, the screen been acting strangely, lines go straight through move the mouse returns to doc, redo button does not light. After an hour or so... I must close Solid Edge for lack of memory. Commands are slow,
Yes, to answer your question... It was to go in for a virus to be removed for being slow, now I have to deal with this!! Yea
Is this computer compatible for Solid Edge?

Re: Computer Issues

KennyG 2nd Gear
2nd Gear
Computer would be fine for small to medium assys. I would run a repair on Solid Edge though...
Sent from my Motorola Electrify using Tapatalk 2


Ken

Production: ST10 MP3
Testing: SE 2019

Re: Computer Issues

N/A
This is what came up first thing this morning.
http://screencast.com/t/u6ncBbR1sB
How do I go about to run a repair on Solid Edge. Also, what do I need to to upgrade to take a larger assy

Re: Computer Issues

KennyG 2nd Gear
2nd Gear
A repair can be done from the add/remove programs form.
You might be able to add more RAM to avoid the memory message, but the version of SE you have is 32 bit thus it is limited to 4GB of virtual address space so you may keep running into the issue.
Sent from my Motorola Electrify using Tapatalk 2


Ken

Production: ST10 MP3
Testing: SE 2019