Could not install solid edge????

N/A
I downloaded the software from its web site but at my 64 bit system with window 7 i could not install it . it show installation wizard inturrepted?
7 REPLIES

Re: Could not install solid edge????

Esteemed Contributor
Esteemed Contributor
Hi there....you may need to try running the installation as the administrator to bypass any control issues from your OS or anti-virus may be trying to exert.
Right mouse button click on the .exe file, and choose "Run as administrator"

Hope that helps.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Could not install solid edge????

N/A
sorry, 'run as admin' aint working. Please help!

Re: Could not install solid edge????

N/A
Are you linking to the license file in the set up dialog? Note this is (optional) If so try to run the install without the license file link...

MANY are having issues renaming the license file and windows naming it a ".txt" file.. this file must be "SELicense.dat"

HTH

Re: Could not install solid edge????

N/A
I downloaded the software from its web site but at my 64 bit system with window 7 i could not install it . it show installation wizard inturrepted?

Me to I am new on the wedsite and I cant find anything

Re: Could not install solid edge????

N/A
I cant find it to morgan the name EAST is my game!!!!!!!!!!!!!

Re: Could not install solid edge????

N/A
what?????????????

Re: Could not install solid edge????

N/A
Dear Forum

My name is Mariano a Computer Aided Design student, thanks for you quick response with the downloading details, but unfortunately I haven’t been able to download the program, it takes a lot of time and when it gets to 70 and above it just says that downloading error and does it, and I try and try and the message keeps repeating, well it has gone the 24 hour validation period and I still try but the same message appear.

Please I need the program as soon as possible as I have so much work to do and due to the dead line I can possibly failed the subject.

Please anything you can help with, in order for me to download the program, will be much appreciated.

Kind Regards

Mariano Ospina Cadavid
LSBU London
ospinam4@lsbu.ac.uk