Creases with Bluedot manipulation of Surface

N/A
Wondering why I'm getting creases when manipulating bluedots with shapedit? the sections are from insert sections option and I notice they have a lot more points than the original sections they were copied from. Is it perhaps something to do with tolerance setting in Bluesurf?

Keith
2 REPLIES

Re: Creases with Bluedot manipulation of Surface

N/A
Yes its the tolerance setting (sorry, it is in the help file).
So, is there a setting that will reproduce a curve with the same number of points as the original?

Re: Creases with Bluedot manipulation of Surface

N/A
Keith,
Smoothing of surfaces in SE is an ongoing challenge for me -
it consumes TOO many hours and leads to great frustration!
Changing the appearance of the part to a highly-reflective fin-
ish (eg Chrome, with Reflections 'on') is helpful in assessing
the actual appearance of the Part (apart from the other anal-
ysis tools available such as Zebra stripes)
The best way to reduce curve-points is to Edit the profile and
use the Simplify tool, setting the allowable deviation from the
existing Curve (I often select a value in the range 0.02 to 0.05
mm) to reduce the number of points and smooth the curve.
HTH,
Rick.

"designerplants@gmail.com"

wrote in message
news:designerplantsgmail.com.59fivo@noreply.bbs.industrysoftware.automation.siemens.com...
>
> Yes its the tolerance setting (sorry, it is in the help file).
> So, is there a setting that will reproduce a curve with the same number
> of points as the original?
>
>
> --
> designerplants@gmail.com
> ------------------------------------------------------------------------
> designerplants@gmail.com's Profile:
> http://bbs.industrysoftware.automation.siemens.com/vbulletin/member.php?userid=405149
> View this thread:
> http://bbs.industrysoftware.automation.siemens.com/vbulletin/showthread.php?t=48534
>