Creating An Angle Better Than -180 Degree

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I Have Drawings That Are Greater Than  A -180°Angles To 180°, My Setting Goes To -180° Down To 0°. 

Is There A Setting Of An Angle To A Reading From -180° To 360°

 

Thank You

Greg

1 REPLY

Re: Creating An Angle Better Than -180 Degree

Esteemed Contributor
Esteemed Contributor

Hi @PO_LC,

 

 

If I understand you correctly, then, YES....there is an option in the command bar toggle, used when placing the dimension, called "Angle Between"....see below

 

ST8_DFT_AngleDimension_AngleBetweenOption.PNG

 

(view in My Videos)

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000