Dimension in mixed fraction

Experimenter
Experimenter

Hi,

I would like to know if is possible to put the dimensions in  mixed fraction like the image attached in solid edge st6

Thanks Smiley Happy

mixed fractionmixed fraction

2 REPLIES

Re: Dimension in mixed fraction

Phenom
Phenom

Hi:

 

It is possible to specify the dimension as a mixed fraction.

For example when drawing a line, click the start point and when specifying the length, simply type 1 5/16 then press TAB

Solid Edge evaluates the mixed fraction value and sets the line length accordingly.

You can even use formulas with simple arithmetic operations when specifying the dimension.

 

 

Re: Dimension in mixed fraction

Esteemed Contributor
Esteemed Contributor

@Malaka91 Yes, you can change the round off format to fractional but it does not show it in stacked format but rather the single line linear format such as "3 1/2".  You can also specify a fraction seperator such as the dash to make it more clear and look like this "3-1/2".



Ken

Production: ST10 MP3
Testing: SE 2019