Download and Installation Problems

Experimenter
Experimenter

Good Morning,

 

I have downloaded The SolidEdge program with academic license (I'm a student).

 

If I try to download the format 64-bit the file starts the download but after a bit time the download is stopped and the "file is corrupt". I tried with differents PC and wifi. Are there any trobles on the site?

 

Instead I can dowload easy the 32-bit . (But probably on pc the 64-bit could be better).

So I have done in this way.

 

I have downloaded and installed correctly the program.

But When I run it on the principale page if I try to open an type of the existing files to start, the program goes to wrong and it will be closed.

 

Can you help me?

 

thanks in advance