Error -88,309

N/A
Runtime error in Solid Edge. See atach please.
6 REPLIES

Re: Error -88,309

SeanCresswell 2nd Gear
2nd Gear
Hi there,

Appears to mention your system clock has been set back. :confused:
Not sure if this is the correct action, but....is your system clock/calender set correctly?
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Error -88,309

N/A
If the date and time are correct.
Thursday September 29, 2011.
I also thought that, but does not work, uninstall the software 10 times.
Delete all the log entries that mention it.
But the problem continues ...

Re: Error -88,309

N/A
Wow, change the date to December 29, 2011 ..
and it works ....
Now I went back to September 29, 2011.
The software works, it gives the same error but it works
I miss, not so much just Windows.

Re: Error -88,309

SeanCresswell 2nd Gear
2nd Gear
Maybe the issue was with the license, not the install file....but you might try going through the entire process again, to ge a fresh license & download link....try with the download you have, if that fails, then re-download the installation file.

But at least you have functioning software now. :cool:
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Error -88,309

N/A
I Have Same error unloaded changed clock no joy. When I cancel the error it says you do not have a valid solid edge license contact you administrator to obtain licence.

I have checked contents of selicence in the programs file and it matches the .txt content I received in email

Re: Error -88,309

N/A
I am experiencing this error as well. Can anybody help me resolve the issue?