Error during installation

Experimenter
Experimenter

Hi, I tried to install ST7 version, but the computer show erro 7021 (ols version already intalled).

How can i uninstall ST4 registers?

 

Regards

jlima

 

1 REPLY

Re: Error during installation

Siemens Phenom Siemens Phenom
Siemens Phenom

From the Solution Center database:

 

Manually uninstalling Solid Edge after failed uninstall

Symptom
---------------
When attempting to uninstall Solid Edge, the uninstall fails and Solid Edge is not fully uninstalled. How to clean up and manually finish uninstalling Solid Edge after a failed uninstall?

Hardware/Software Configuration
Solid Edge

Solution
If you have issues with uninstalling Solid Edge then you will need to perform a manual uninstall:

1. Manually delete the Solid Edge program folders typically in C:\Program Files or C:\Program Files (X86).

2. Manually delete the Solid Edge user preference folder %APPDATA\Unigraphics Solutions.

3. Manually clean up the registry by deleting any Solid Edge registries in the following locations:

HKEY_CURRENT_USER\Software\Unigraphics Solutions

HKEY_LOCAL_MACHINE\Software\Unigraphics Solutions

HKEY_LOCAL_MACHINE\Software\Wow6432Node\Unigraphics Solutions

4. Reboot the workstation.

Solid Edge should now be completely uninstalled and ready to reinstall Solid Edge.