Error while working with 3d objects

N/A
Hi. I am having an issue while creating 3d object. To be honest im quite fresh to the the program, however I've been working with some of those kind for some time.
Right in the moment when i add 3rd dimension to an object, there appears an error, forcing me to exit the program.
Found Crash-log file so uploaded it right here:
http://speedy.sh/tJsPv/crashlogf.txt
Working at net-book acer aspire, not saying its perfect but should be enough to carry on the operations done.
I'm not an expert, and hope anyone to help me solving the issue, as i need to have some work done soon. Thanks in advance.
1 REPLY

Re: Error while working with 3d objects

Esteemed Contributor
Esteemed Contributor
Hi there,
I would suspect that the lack of sufficient available physical memory is one of the issues....possibly also the graphics adaptor.
Not really an application that one would typically use on a net-book. You would have to disable a raft of display settings to unload the system resources required.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000