Extrusion Problem

Creator
Creator

We are having a problem making an extrusion on the attached part.  We are trying to connect the base to the top of the part and we are getting a message that says zero thickness (non-manifold) body.  I've attached a screen shot and the file itself.   I was wondering if someone could point us in the right direction?  Thank you.

 

TRC

1 REPLY

Re: Extrusion Problem

Esteemed Contributor
Esteemed Contributor

Hi there,

 

I think I know whats going on here, but can't quite see which portion is the main cause from the image.....would you please upload your model as a Parasolid file?...as my commercial version of Solid Edge cannot open your Student Edition file. [works commercial back to you though]

Also,....in order to transmit your problem geometry, could you make a surface from the curve set before exporting it to Parasolid? [you may also need to check the option for "Export Sheets", to get it through with the existing solid geometry

 

ST8_PAR_SaveAs_Translated_Parasolid_Options_Sheets.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000