File Corrupt (even after the 7th try)

N/A
I have tried downloading the student version of solid edge 7 times (using my 3 different email addresses/links).
but the closest it got me was to 70% 'extraction' before saying its corrupt, Again!
I have tried using a download manger, and tried it using google crome, firefox, and explorer.
My download speed had been averaging at 1.4Mb/sec (during the download), so i dont think the speed is the problem.

If anyone can help, i would love the help, before uni starts up again.

Cheers
3 REPLIES

Re: File Corrupt (even after the 7th try)

N/A
Try using the download manager with "binary" mode for download. That worked for me.
I used "Free Download Manager".
Right-click on download -> Download properties.
Go to Protocol Tab, under "Transfer mode" section
Click on "Binary", Then click Ok.
I had to try several times as well, until I realized that it was probably downloading in ASCII which meant it didnt download completely correctly. Downloading in "binary" mode ensures a more exact copy. Try it and see if it works.

Re: File Corrupt (even after the 7th try)

N/A
thanks for the idea, but sadly after downloading using 'binary' twice, and trying to 'extract' each of the downloads twice, it still only makes it to 85% before saying its corrupt. Smiley Sad
22GB later, and still no luck.
any other ideas?

Re: File Corrupt (even after the 7th try)

Siemens Phenom Siemens Phenom
Siemens Phenom
Try using this direct download link:
http://dl2.plm.automation.siemens.com/solidedge/SolidEdgeV105ENGLISH_32Bit.exe
-Dave

On 04/02/2013 12:36, 16515895@student.uws.edu.au wrote:
>
> thanks for the idea, but sadly after downloading using 'binary' twice,
> and trying to 'extract' each of the downloads twice, it still only makes
> it to 85% before saying its corrupt. Smiley Sad
> 22GB later, and still no luck.
> any other ideas?
>
>