Healing the Wounds Failed

N/A
What is it men't by healing the wounds with deleting holes, Also there is required a hole that is to be inserted in the part 1.875 in.length x .125 in dia. If tried with finding an edge to the part to flip. nothing.

http://screencast.com/t/JqPGK2acl

Thanks
Crousie
1 REPLY

Re: Healing the Wounds Failed

N/A
try to detach the hole and then delete it.

the message means that when the hole is deleted SE can not heal the open faces, most likley becasue this hole crosses over the tangent line of the round.