Help for Solid Edge ST6!

N/A
I recently downloaded and installed the SE ST6. Everything was going fine until I tried opening the Solid Edge ST6 program itself. It is asking me for a key and I do not know what to do. I tried using the file saved as SELicense.dat but it just constantly keeps saying I do not have a connection to the license fileserver. Invalid License File Syntax, flexnet licensing error -2413. Detailed instructions would be really helpful.
2 REPLIES

Re: Help for Solid Edge ST6!

PLM World Member Legend PLM World Member Legend
PLM World Member Legend
Make sure your license file has a .dat extension and not .txt Sometimes
the files are distributed with a .txt extension even though this doesn't
work.
That's all I can think of.

On 14/01/2014 03:34, wk12498@gmail.com wrote:
>
> I recently downloaded and installed the SE ST6. Everything was going
> fine until I tried opening the Solid Edge ST6 program itself. It is
> asking me for a key and I do not know what to do. I tried using the file
> saved as SELicense.dat but it just constantly keeps saying I do not have
> a connection to the license fileserver. Invalid License File Syntax,
> flexnet licensing error -2413. Detailed instructions would be really
> helpful.
>
>

--
Dr Frank Mill CEng FIMechE <>
Schoolof Engineering
Sanderson Building <>
Universityof Edinburgh
King's Buildings
Edinburgh
Scotland
EH9 3JL
tel++44 (0)131 650 5673
skypeshandonfrank or ++44(0)131 208 1642
mob++44 (0)7974 650892
Edinburgh University

Re: Help for Solid Edge ST6!

Esteemed Contributor
Esteemed Contributor
Further to Franks info....make sure you have file extensions displayed, as if they're hidden you'll not be correcting the extension but merely appending it.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000