I cant reinstall solid edge

N/A
i was trying to activate my solid edge license and i could not access the solid edge license utility because it said it was already running when it wasn't. so i uninstalled it to attempt to reinstall it, but when i re install it the program says i have solid edge installed already but i don't any help?
4 REPLIES

Re: I cant reinstall solid edge

N/A
Verify that indeed SE in not installed:Controll Panel --> add/remove software

Then delete the SolidEdge Registry before you try to re-install.
HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge

HTH

Re: I cant reinstall solid edge

N/A
it is confirmed that its is indeed uninstalled from my computer and it is not on my registry and it is still not allowing me to install solid edge

Re: I cant reinstall solid edge

N/A
Have you rebooted the PC? Do a restart and allow it to release anything it may be holding form the uninstall .. Sometimes shared Dlls cant be released until a reboot?

Did you manually remove the registry? It will not just be gone from the uninstall you have to do so manually.

I would try once again these steps:

1.) stop everything and reboot PC
2.) Control Panel --. add/remove
3.) If Solid Edge is found try repair and then remove
4.) reboot
5.) manually remove HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge
6.) reboot
7.) try to install fresh

if this does nto work... I'm lost...

good luck

Re: I cant reinstall solid edge

N/A
no luck at all im re downloading the installer now maybe that will help. thanks for the help.