Insert Object cmd missing in Ordered mode

Valued Contributor
Valued Contributor

Hello everyone!

I cannot find the insert object command on Ordered mode. Also I have tryied writing it on the command line, but I´ve got no luck yet. I am wondered why is it only available on the Sync mode. It will be really helpful if anyone can give me an explanation!

 

Thank you

4 REPLIES

Re: Insert Object cmd missing in Ordered mode

Esteemed Contributor
Esteemed Contributor

Hi there @AmanRa,

 

In "Ordered", you place an OLE [Text & Image] from within the "Sketch" mode, either independently, or at feature creation. [go to Sketch..."Tools" tab, on the "Insert" group]

 

ST9_PAR_Ordered_Tools_Insert.png

 

......where as in "Synchronous", sketching resides in the same live modeling environment as your features.

 

ST9_PAR_Synchronous_Sketching_Insert.png

 

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Insert Object cmd missing in Ordered mode

Valued Contributor
Valued Contributor
Just a quick question. Where can I find this option on ST8? Thanks for the information, really useful.

Re: Insert Object cmd missing in Ordered mode

Esteemed Contributor
Esteemed Contributor

Are you referring to Insert Image?  Not sure Insert Object is available anywhere but in Draft.

 

If so, it is because you have to insert the image within a sketch.  Since Synchronous' sketches are modeless the Insert Image command is always available.  Since Ordered's sketches are modal the Insert Image command is not available until you are in the Sketch mode.



Ken

Production: ST10 MP3
Testing: SE 2019

Re: Insert Object cmd missing in Ordered mode

Valued Contributor
Valued Contributor
Thank you! I´ve got what I wanted. Thanks!