License incorrect

N/A
The license come with the email, but no one is correct and also the sign up link is dead.
Please Help!
3 REPLIES

Re: License incorrect

N/A
MY license
INCREMENT solidedgeacademic selmd 104.0 01-jun-2013 uncounted \
VENDOR_STRING="SOLID EDGE ACADEMIC COPY" HOSTID=DEMO \
ISSUER=SIEMENS SIGN="1A40 E605 46F6 E288 765D 94F8 63E4 BE2F \
3EE9 2A4A 1BEC 2657 8339 29C8 4117 1DA8 6256 6B5B 1A14 1040 \
1781 5AB7 40B5 930C AE22 FB2A 4198 7405 F2D1 666D"

Re: License incorrect

uk_dave 1st Gear
1st Gear
The license file you provides works without issue on my machines.
If you have the option to “hide extensions for known file types� turned
on in your Windows Explorer options then more than likely you have
simply incorrectly named your license file to something like
“SElicense.dat.dat� or “SElicense.dat.txt� and do not know it. Turn the
option on to display file extensions in Windows Explorer and make sure
that you have correctly named the license file to “SElicense.dat� and
placed it into the C:\Program Files\Solid Edge ST5\Program folder location.
-Dave
On 22/10/2012 17:22, mundycho@gmail.com wrote:
>
> MY license
> INCREMENT solidedgeacademic selmd 104.0 01-jun-2013 uncounted \
> VENDOR_STRING="SOLID EDGE ACADEMIC COPY" HOSTID=DEMO \
> ISSUER=SIEMENS SIGN="1A40 E605 46F6 E288 765D 94F8 63E4 BE2F \
> 3EE9 2A4A 1BEC 2657 8339 29C8 4117 1DA8 6256 6B5B 1A14 1040 \
> 1781 5AB7 40B5 930C AE22 FB2A 4198 7405 F2D1 666D"
>
>

Re: License incorrect

SeanCresswell 2nd Gear
2nd Gear
Further to Dave's advice.....it is the entire file that needs to be used, NOT any individual part of the content. Solid Edge will read from it at every start up.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000