MP download mit Studenten Version

Experimenter
Experimenter

Hi Community,

 

ist es möglich das ih mit meiner Studenten Version die MPs downloaden kann?

Ich habe Windows 10 und ST7 und angeblich soll ST7 unter Windows 10 ab dem MP 4 und höher laufen!

 

Mit freundlichen Grüßen

 

Dennis

7 REPLIES

Re: MP download mit Studenten Version

Esteemed Contributor
Esteemed Contributor

Gyno wrote:

Hi Community,

 

it is possible that IH can download the MPs with my student version?

I have Windows 10 and ST7 and allegedly ST7 10 run on Windows from the MP 4 and higher!

 

Yours sincerely

 

Dennis


 

 

Hi Dennis,

 

No.....the maintenance packs are only available to commecial users on "current" paid annual maintenance.

 

As yet Windows 10 is not supported, in any of the current [nor previous] versions of Solid Edge....although, some users [on commercial licenseshave done so, and reporting their success, it is not yet recommended to upgrade to Win10.

 

If Siemens were to update the existing application,....I suspect they would most likely replace the software package on their server, and users would then need to re-download it and the completely uninstall & reinstall Solid Edge.

[Also note: these are only my thoughts....I don't work for Siemens, and nothing official has been said to this effect]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: MP download mit Studenten Version

Esteemed Contributor
Esteemed Contributor

Hi there,

 

This thread might be of help to you..... >here<

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: MP download mit Studenten Version

Siemens Phenom Siemens Phenom
Siemens Phenom

@Gyno

The Solid Edge ST8 Student Edition download is available now for you to download.  It just posted within the past few minutes.

 

Please note that we are not aware of any serious problems running ST8 on Windows 10, but our testing is still underway and Solid Edge support running on Windows 10 has not been officially announced yet.

 

Please be sure that 3.5 .net (also required with ST7) remains installed on the machine.

 

Enjoy,

Laura

Solid Edge Release Manager

Re: MP download mit Studenten Version

Experimenter
Experimenter

@LauraWatsonwo kann ich denn ST8 downloaden? Funktioniert das mit meiner Studenten Version?

 

Mit freundlichen Grüßen

 

Dennis

Re: MP download mit Studenten Version

Siemens Phenom Siemens Phenom
Siemens Phenom

@Gyno

You can download the ST8 Student Edition here:

http://www.plm.automation.siemens.com/en_us/academic/resources/solid-edge/index.shtml

 

You will register and select the language of Solid Edge ST8 and receive a license key via email.

 

Laura

Re: MP download mit Studenten Version

Experimenter
Experimenter
Danke für die schnelle antwort @LauraWatson

Ich werde versuchen ST8 auf Win 10 zu installieren!
Neuigkeiten folgen in kürze

Re: MP download mit Studenten Version

Experimenter
Experimenter

Mein Feedback @LauraWatson

 

ST8 läuft mit net 3.5

 

Danke für die Hilfe