No licence download?

N/A
I cannot locate a valid licence file and am therefore unable to complete the download.
3 REPLIES

Re: No licence download?

Pioneer
Pioneer
When you recieved the email for the download link after registering, there was a SELicense.txt file attached, which is the license you need to point to when running the License wizard after loading Solid Edge.

Re: No licence download?

N/A
I cannot locate a valid licence file and am therefore unable to complete the download.




Read this and try the link that i have given...

Siemens ask for student registration before downloading. After registration, they send a link to your email id and also SE License.txt as an attachment to the same email. The link provided into email from Siemens is valid for download in 24 hours only : just check that link carefully... it will contain following link as a part of download link...

if you want to download solidedge st4 directly and in more than 24 hours(especially when using low speed internet), then use this link (paste it in browser address bar) :

http://dl2.plm.automation.siemens.com/solidedge/SolidEdgeV104ENGLISH_32Bit.exe

address in above link (after http://) dl2.plm.automation.siemens.com/solidedge/SolidEdgeV104ENGLISH_32Bit.exe

and don't forget to get valid student license for above copy of st4, by registering yourself on siemens website... ignore if u have received license... license file do not have 24 hr restriction....

hope you will be able to download st4 now...

Re: No licence download?

N/A
I have received the download link but no license file was attached. Only a strange sequence of random letters in the last line of the message.
I have also checked the junk folder but it was empty. Could you resent license file?

Thank you.
-Per