Octagon Out Of Dimensions

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I've noticed the octagon center point is out. Have a typed dimension say 4.091 and the end result is 4.724. I have to go back to Smart dimension to adjust the right dimension. 

Any thoughts

 

Greg

5 REPLIES

Re: Octagon Out Of Dimensions

Esteemed Contributor
Esteemed Contributor

I would say it's more likely to be your placement point that is out, rather than the center point of the polygon geometry.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Octagon Out Of Dimensions

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor
With this short video... Showing the octagon out of dimension all around.
Is there a reset to send back to standard.

http://screencast.com/t/r4tRjFw9LuWh

Greg

Re: Octagon Out Of Dimensions

Community Manager Community Manager
Community Manager

Look at your command bar -- there are two options -- measure to corner or measure to flat. You are set to measure to flat. Change it to measure to corner and I think you will get the result you expect.

Dan Staples
Director, Solid Edge Product Development

Re: Octagon Out Of Dimensions

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I've noticed the only time the dimension is in sinc is a new documents. 

With this video in an existing document shows an out of dimension octagon.

 

http://screencast.com/t/IHFL746q

Greg

Re: Octagon Out Of Dimensions

Experimenter
Experimenter

Whenever you enter a dimension for the polygon, you are not entering the dimension for the chord. Rather, the distance from the polygons center to the midpoint of the polygons chord (or the vertex depending on which option you have checked in the command bar) So, in your case if you get your Smart Dimension tool and first click on the center point of the polygon, then click on the midpoint of the chord, you will get the distance you originally entered.

 

-Preston