Problem Downloading/Installing ST5 Student Version

N/A
I got a download link through me email, and was able to save the license no problem, but I can't seem to complete the download on the 2GB exe file through the link.
I download seems to eventually stop itself with an incomplete file. One of the times after 17 hours the file made it to 1.99GB before stopping. When I tried to install with it I got a FILE CORRUPT error message.

Is there some other link or mirror I can use to get the exe file and apply my license to it? Or is there some better way to make sure this download successfully completes?

Thank you very much in advance for your help!
2 REPLIES

Re: Problem Downloading/Installing ST5 Student Version

Esteemed Contributor
Esteemed Contributor
Hi there Issac,
Try using this direct link to the download file.....you will still need to have your license file saved to a handy location on the PC your installing SE on.
http://dl2.plm.automation.siemens.com/solidedge/SolidEdgeV105ENGLISH_32Bit.exe
Reply here if you have any further issues or comments.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Problem Downloading/Installing ST5 Student Version

Esteemed Contributor
Esteemed Contributor
Also, I would recommend using a Download tool like Internet Download Manager (paid) or Download Accelerator Plus (free). They will speed up the downloads as well as will be "connection loss" tolerant and they can also typically resume incomplete downloads (depends on server but most support it, including Siemens PLM)

Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3