Problem with Solid Edge License

N/A
Hey,
I installed a Solid Edge and now when I want to enter to a Solid Edge he say me that I have no license.
I read what I got in E-mail (how to do license), but now when I'm trying to enter to a Solid Edge open some window with the problem:

((http://www.myg.co.il/index.php?loc=see&pic=phpFXBUyD.png))

Please.. someone can help me?
15 REPLIES

Re: Problem with Solid Edge License

N/A
i istal st4 in xp 3 . but steel lience problem is occure pls help

Re: Problem with Solid Edge License

N/A
Someone can give me a Key for Solid Edge?
Please, I very need this Key, because I wanna to start use with a Solid Edge ..

Re: Problem with Solid Edge License

N/A
Form other threads on this forum:
To apply the license after installing Solid Edge
1. Save the electronic file to a convenient location. The default
filename will be SELicense.txt.
2. Start the License Utility (located in the Solid Edge program group on
the Start Menu in the Licensing section).
3. Next click "Browse" in the dialog box, and navigate to the file. You
may need to change the file type in the License Utility to *.* to locate
the license file with .TXT file
4. The License Utility program will automatically copy the file to the
Solid Edge Program folder.
5. You should be able to run Solid Edge, look for it on the Windows
start menu and launch the application.
And
Try renaming the license file from SELicense.txt to SELicense.dat. Make
sure it is not SELicense.dat.txt as Windows does love to add extensions
if you have them hidden in the folder options.
Then save it in your C:\Program Files\Solid Edge ST4\Program folder.
You should overwrite the existing file.

On 2/29/2012 11:57 AM, georgipav1996@gmail.com wrote:
> Someone can give me a Key for Solid Edge?
> Please, I very need this Key, because I wanna to start use with a Solid
> Edge ..
>
>

Re: Problem with Solid Edge License

N/A

Try renaming the license file from SELicense.txt to SELicense.dat.

Renaming the license file in "License Utility", in the dialog box near the "Browse"?

Re: Problem with Solid Edge License

N/A
Nope, just use Windows Explorer but make sure that you do *not* have
hide file extensions enabled in explorer otherwise the file will become
named SELicense.dat.txt
On 2/29/2012 12:18 PM, georgipav1996@gmail.com wrote:
> David Merritt;219186 Wrote:
>>
>> Try renaming the license file from SELicense.txt to SELicense.dat.

> Renaming the license file in "License Utility", in the dialog box near
> the "Browse"?
>
>

Re: Problem with Solid Edge License

N/A
http://www.myg.co.il/index.php?loc=see&pic=phpZrLDNK.png
I clicked on "Browes" in the dialog box and navigated to the file.
Now I can click on "OK"?

And I didn't understand how to rename the file "SELicense.txt" ..

Re: Problem with Solid Edge License

N/A
yes click on OK.
On 2/29/2012 12:50 PM, georgipav1996@gmail.com wrote:
> http://www.myg.co.il/index.php?loc=see&pic=phpZrLDNK.png
> I click on "Browes" in the dialog box and navigated to the file.
> Now I can click on "OK"?
>
> And I didn't understand how to rename the file "SELicense.txt" ..
>
>

Re: Problem with Solid Edge License

N/A
Die Uhr in Bios war falsch eingestellt.
Ich habe es gut gemacht, dann
habe ich Nachricht bekommen
"Systemclock has been set back"
...
FlexnetLicensing Error:-88,309
Was kann ich damit zu tun?
What can I do with Error Message?
Danke/Thanks

Re: Problem with Solid Edge License

N/A
After clicking OK, it says "You may not have write-access to the file or dictionary". I am an administrator on my own computer... What should I do?