Problems with installing ST5 Student Edition

N/A
Hello there.

I would have the following problem: I've tried installing ST5, and when I click the "Install Solid Edge ST5", the moment it would start installing, it says something along the lines: the program installation has been interrupted, the system settings have not been changed. I'm running W7 64 bit. My gpu drivers are up to date, and I'm running a GTX 260 M on my laptop (however I doubt any of this could influence the installation process).

I've seen a few tutorials and would really love to give this software a try.

Thank you for the time and effort.
31 REPLIES

Re: Problems with installing ST5 Student Edition

Esteemed Contributor
Esteemed Contributor
Hi there.....I suspect that either, the actual download file is corrupted, or you need to "right click" on the install file and choose "Run as administrator".
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Problems with installing ST5 Student Edition

N/A
I've downloaded it thrice, and doesn't make any difference. Also, UAC is off (I've read the instructions on the installation pdf). Ran it as admin, had similar problems and running it as such usually helped, not in this case though.
Any other suggestions perhaps?

[langtitle=es]Re: Problems with installing ST5 Student Edition[/langtitle]

N/A
A mi me pasa lo mismo y no se que hacer

Re: [langtitle=es]Re: Problems with installing ST5 Student Edition[/langtitle]

Esteemed Contributor
Esteemed Contributor
Sounds like a Windows Installer issue. Which version of Win 7 are you running?


Ken

Production: ST10 MP3
Testing: SE 2019

Re: [langtitle=es]Re: Problems with installing ST5 Student Edition[/langtitle]

N/A
windows 7 home premium de 64 bits y service pack 1

Re: [langtitle=es]Re: Problems with installing ST5 Student Edition[/langtitle]

Esteemed Contributor
Esteemed Contributor
Specifying ISO templates? If so, try ANSI and see what happens.


Ken

Production: ST10 MP3
Testing: SE 2019

Re: [langtitle=es]Re: Problems with installing ST5 Student Edition[/langtitle]

N/A
He probado con ANSI y me pasa lo mismo, al darle a instalar, me dice que se ha interrumpido la instalacion

Re: [langtitle=es]Re: Problems with installing ST5 Student Edition[/langtitle]

N/A
refresh, I have the same problem

Re: [langtitle=es]Re: Problems with installing ST5 Student Edition[/langtitle]

N/A
Same problem here.
Win7 Professional, SP 1, 64bit.
"File is corrupt"