ST2 and ST4 on one PC?

N/A
Hello,

i would like to know if its possible to run Solid Edge ST2 and ST4 on one PC, Operation System is Windows 7 Professional 64 Bit, ST2 is a 64 bit Version, the ST4 32 bit.

Thanks in advance
3 REPLIES

Re: ST2 and ST4 on one PC?

N/A
No. SE only supports one version installed.
Ken
http://grundey.blogspot.com
http://www.pella.com

On 11/30/2011 4:51 AM, C_Grebner@web.de wrote:
> Hello,
>
> i would like to know if its possible to run Solid Edge ST2 and ST4 on
> one PC, Operation System is Windows 7 Professional 64 Bit, ST2 is a 64
> bit Version, the ST4 32 bit.
>
> Thanks in advance
>
>

Re: ST2 and ST4 on one PC?

N/A
Thank you for the quick response, but do you if its possible to run SE in a VM maybe unter Windows 7 or XP?

Re: ST2 and ST4 on one PC?

N/A
It's possible, but would not recommend it. Depending on the VM, it may
not support hardware graphics so the display will be horrible.
Ken
http://grundey.blogspot.com
http://www.pella.com

On 12/6/2011 4:51 AM, C_Grebner@web.de wrote:
> Thank you for the quick response, but do you if its possible to run SE
> in a VM maybe unter Windows 7 or XP?
>
>