ST4 instead of ST5

N/A
Hi,

is there any possibility to use ST4 instead of ST5?
Maybe someone could provide a download link. (?)
Will this work with my current licence for ST5?

Thanks.
8 REPLIES

Re: ST4 instead of ST5

Esteemed Contributor
Esteemed Contributor
Hi there,
The license file is backward compatible, but that only helps if you have the older "SolidEdgeV104ENGLISH_32Bit.exe" file, or are already running ST4 Student Edition.
I'm puzzled though,....as to why you would NOT want to use the most current version of Solid Edge?
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: ST4 instead of ST5

N/A
Hi,
thanks for your answer.
The reason is our university. There we use version ST4 and also our exam will be with ST4.
Thats why I want to use ST4, so I don't have to worry that some (little) things have changed.

Re: ST4 instead of ST5

Esteemed Contributor
Esteemed Contributor
OK...well then, I would hope that the university can provide the application to you on a flash drive or DVD.
Siemens is OK with sharing the application out....everyone just needs to register to get their license file.
I have them both saved away at home for my sons laptop...he has given it to all his like minded friends.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: ST4 instead of ST5

Esteemed Contributor
Esteemed Contributor
I remembered I posted the link in an earlier post and wondered if it might still be active.....just tried, and it was ready to start, so ST4 version must still be on the server.
Go here... http://www.plm.automation.siemens.com/app/dl/SolidEdgeV104ENGLISH_32Bit.exe
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: ST4 instead of ST5

N/A
Hi,
thanks!
Download started ... Smiley Happy

Re: ST4 instead of ST5

Legend
Legend
Hi Sean,
When the versionnumber is changed to 105 you can download the ST5 version
also from the address you supplied below.

ST4
http://www.plm.automation.siemens.com/app/dl/SolidEdgeV104ENGLISH_32Bit.exe
ST5
http://www.plm.automation.siemens.com/app/dl/SolidEdgeV105ENGLISH_32Bit.exe
Kind Regards,

Jan Bos
The Netherlands
"SeanCresswell"
wrote in
message
newsSmiley FrustratedeanCresswell.5l7nuz@noreply.bbs.industrysoftware.automation.siemens.com...
>
> I remembered I posted the link in an earlier post and wondered if it
> might still be active.....just tried, and it was ready to start, so ST4
> version must still be on the server.
> Go here...
> http://www.plm.automation.siemens.com/app/dl/SolidEdgeV104ENGLISH_32Bit.exe
>
>
> --
> *-*
>
> SE-ST5_MP1
>
> *Sean Cresswell*
> sean@streetscape.co.nz
> (on 'facebook' (http://www.facebook.com/sja.cresswell)) (on 'twitter'
> (http://twitter.com/#!/sean_cresswell))
>
> Manager - Design Office
> ::'STREET*SCAPE* Ltd' (http://www.streetscape.co.nz) ::
> '& The Stainless Factory' (http://www.stainlessfactory.co.nz)
>
> Tauranga, New Zealand, 3110
> ------------------------------------------------------------------------
> SeanCresswell's Profile:
> https://bbs.industrysoftware.automation.siemens.com/vbulletin/member.php?userid=215489
> View this thread:
> https://bbs.industrysoftware.automation.siemens.com/vbulletin/showthread.php?t=50552
>

Re: ST4 instead of ST5

Esteemed Contributor
Esteemed Contributor
Thanks Jan,...that's what I remebered, and so I went looking.
I just wasn't certain it would still work, until I tried it. Smiley Wink
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: ST4 instead of ST5

N/A
Hi guys i was wondering if there's any way to download 64bit of solid edge student edition (regardless of St4 or St5)

I just upgraded my windows to 64bit