ST6 Academic x64

Experimenter
Experimenter

Good evening!

 

As preparation for our next test in professional school, i am currently installing ST6 (32-bit). This is the same version we have on our school computers installed and thus recommended by our teacher.

 

My question: Is there also an ST6 64-bit edition available? I have the 4930k CPU and 16 GB of RAM and do not want to waste ressources. I am running Windows 10, but installing into a VM (VirtualBox) would be an option, if it will run fast enough.

 

Kind regards,

Patrick

1 REPLY

Re: ST6 Academic x64

Esteemed Contributor
Esteemed Contributor

Hi there @pbl,

 

ST6 is not compatible with Windows 10.....as far as I know, the downloadable Solid Edge "Student Edition" was only ever offered in 32bit up until ST6. Now, there is only 64bit available, from ST7 onward...

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000