Section not "Sectioning"

N/A
In the assembly I need to section a construction to expose a bolt inside for a technical drawing. There are two plates and a nut that the bolt is inserted through, yet the section option only cuts one of the plates OR the nut no matter what I do. I need it to cut through all the 4 parts to expose the bolt inside the plates and the nut...

There must be SOMETHING I'm missing, because it works just fine on the university lab computers, but it just won't work for me back home :/
3 REPLIES

Re: Section not "Sectioning"

Esteemed Contributor
Esteemed Contributor
So are you using the PMI section in the Assembly file to do this or are you creating a Section View in the Draft file to do this?


Ken

Production: ST10 MP3
Testing: SE 2019

Re: Section not "Sectioning"

N/A
I am using the PMI Section option, and I have no idea why it doesn't work properly...

Re: Section not "Sectioning"

Esteemed Contributor
Esteemed Contributor
If using ST6, create a video and upload to YouTube and paste the link here. It will help with the diagnosis.
Sent from my Motorola Electrify using Tapatalk 2


Ken

Production: ST10 MP3
Testing: SE 2019