Some basic problems

N/A
I am using solid edge student edition.i am almost new to this.Can someone tell me-

> how i can write inside the solid edge?( i mean, anything that i am making,how can i write on that?)
> From where i can colour and change background?

thats all for now.i gonna come up with some more basic problems. Till then thanks everyone if someone could help me.
8 REPLIES

Re: Some basic problems

N/A
Hi, there are various ways you can write text onto a part model or similar. You could use a sketch on a face, projected sketch geometry or even place an image (JPG, BMP, etc) or logo onto a face using various different methods. Perhaps you can elaborate on what you want to achieve here.

To change the colour of the modelling background you can do the following:
Go to the View Ribbon and choose the View Overrides command in the Style group.
Then on the background tab of the dialogue that appears, simply choose the background options you want. The default is probably set to a gradient so you can play around with the colours you have available in the same tab.

If you set the Type to Solid Edge Default, the colour of this is set within your Solid Edge options dialogue. This is launched from the Application menu at the top left of the screen.

Hope that helps
Jon

Re: Some basic problems

N/A
Tanzin,
There is a function in the Profile environment called Text Profile.
This allows you to create 'written' geometry in editable form
using standard Windows fonts, which can then be used to create
(eg) a cutout (debossed feature) or protrusion (embossed) on
your part.
Text Profile can be made to follow a line or curve but it has a
'cussed' nature and will sometimes flip upside down etc ...
Rick.
"tanzin.k@gmail.com"
wrote
in message
news:tanzin.kgmail.com.502y7n@noreply.bbs.industrysoftware.automation.siemens.com...
>
> I am using solid edge student edition.i am almost new to this.Can
> someone tell me-
>
>> how i can write inside the solid edge?( i mean, anything that i am

> making,how can i write on that?)
>> From where i can colour and change background?

>
> thats all for now.i gonna come up with some more basic problems.
> Till then thanks everyone if someone could help me.
>
>
> --
> tanzin.k@gmail.com
> ------------------------------------------------------------------------
> tanzin.k@gmail.com's Profile:
> http://bbs.industrysoftware.automation.siemens.com/vbulletin/member.php?userid=344518
> View this thread:
> http://bbs.industrysoftware.automation.siemens.com/vbulletin/showthread.php?t=46464
>

Re: Some basic problems

N/A
Hi

I have SE Student Edition and Windows 7,
Could you help me on these questions, 1) how can I delete my changes and mistakes.
2) and Select button does not work with mouse right click in ISO Draft.
How can I fix those problems?


Best regards Tanel

Re: Some basic problems

N/A
You may need to clarify your questions as they seem a bit vague..
1) I have no clue what you are asking
2) Not really sure what you are asking, but the Left Mouse Button is
used to Select...
Ken
http://grundey.blogspot.com
http://www.pella.com

On 9/21/2011 1:17 PM, tanel254@gmail.com wrote:
> Hi
>
> I have SE Student Edition and Windows 7,
> Could you help me on these questions, 1) how can I delete my changes and
> mistakes.
> 2) and Select button does not work with mouse right click in ISO Draft.
> How can I fix those problems?
>
>
> Best regards Tanel
>
>

Re: Some basic problems

N/A
hi

How I can delete? I can´t find button for this.
If I want delete some part, I need to activate with clicking on this part. If I do right click on this part then nothing hapen´s.

my english.......sorry

Tanel

Re: Some basic problems

N/A
And If I do select or select all then also nothing hapen´s.


Help please, homework waiting.

Tanel

Re: Some basic problems

N/A
You should be able to just hit the delete key on your keyboard when you have geometry selected. It will delete whatever you do have selected.
If you're in the draft environment and don't seem to be able to select anything, do you have your select filter set correctly.
Its the button that appears on the left hand end of the floating ribbon. Called Select Options.
You want to make sure you have the 'All Layers' option checked as well as everything else.
Hope that helps

Re: Some basic problems

N/A
Thank You

Problem solved.