Standard Part library

N/A
Hey, I have now downloaded and installed the academic version of solid edge and everything works fine but now I have the problem that I can´t find a library for all the standard parts.... you know nuts, bolts etc.

where could I get such a library?
5 REPLIES

Re: Standard Part library

Pioneer
Pioneer
There is a small library of Free standard parts included with the product. From the menu where you loaded Solid Edge (or you can run the executable again to get the menu) you need to load the "Standard Parts Administrator". Be sure to choose the option to load the Master Part Files. After that you should be able to add any included standard parts. See Solid Edge HELP for further instructions on how to use it.

Re: Standard Part library

N/A
after installation SE Standard Parts Administrator ..file SMAPINIFile.sac is missing in c:\Solid Edge Standard Parts directory
any ideas..? thanks

Win 7 Professional x64 SP1

Re: Standard Part library

N/A
Hi

I have SE Student Edition and Windows 7,
Could you help me on these questions, 1) how can I delete my changes and mistakes.
2) and Select button does not work with mouse right click in ISO Draft.
How can I fix those problems?

Best regards Tanel

Re: Standard Part library

N/A
I believe you have to run the configuration wizard after it is installed
and after configuration is complete, a SAC file should be created.
Ken
http://grundey.blogspot.com

On 9/14/2011 11:03 AM, Martin.Tasek@fs.cvut.cz wrote:
> after installation SE Standard Parts Administrator ..file
> SMAPINIFile.sac is missing in c:\Solid Edge Standard Parts directory
> any ideas..? thanks
>
> Win 7 Professional x64 SP1
>
>

Re: Standard Part library

N/A
of course .. now i have solved this by updating msvcr71.dll
and make clean reinstall --> sac file is generated