Technical Problems with SE on Win10

Creator
Creator

Hey everyone,

i would like to know if any of you ran into the same Problems as i am currently.

I´ve got the Problem, that Solid Edge ST9 pretty much always crashes when i have a part opened and then try to resize the Window or maximize it by moving it against the top of the screen.

Im Running Solid Edge on Windows 10.

Im not getting any Error messages on crash the Program only freezes and i have to force close it via task manager.

1 REPLY

Re: Technical Problems with SE on Win10

Esteemed Contributor
Esteemed Contributor

Probably caused by your graphics system on your PC.  What graphics card/chipset are you using and do you have the latest driver installed?

 

You can attempt to turn off the Automatic graphics settings in Solid Edge Options and then manually set the setting to Backing Store to see if that resolves the issue.



Ken

Production: ST10 MP3
Testing: SE 2019