Showing results for 
Search instead for 
Did you mean: 

Thread Size Specification


I am in the process of completing a ful working drawing project for my first year Engineering course. Having used Solid Edge in highschool many years ago I decided to use it instead of the extremely outdated 2D IntilliCAD system used at my University. It trying to create a screw for the project I have come upon a troubling problem. The thread size specified in the drwaing for replication is a M10x1.5 course fit. However, Solid Edge seems to only carry a Fine Fit Library for its thread sizes. I do see that there is a Tetrahedral Thead size for M10x1.5, but thats not what im looking for. Where can I either, set a custom size or add the the directory?


Re: Thread Size Specification

you can add thread definition in the Hold DB...   see the SE help


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.6