Using Protrusion For A Line, Curve

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Short Question,

Is It Possible To Use Line, Curve Or Arc Without A Region To Create A Protrusion.

I Noticed On The Prutrusion There Are Commands For A Single Line, Chain, And Face.

 

Using The Single Protrusion Command In Solid Edge... Can A Protrusion Be Used On A Line.

 

Thanks

GregoryLee

 

1 REPLY

Re: Using Protrusion For A Line, Curve

Esteemed Contributor
Esteemed Contributor

Hi Greg,

 

Yes, but not as the first feature [except in Sheet Metal >PSM<]...as Solid Edge will automatically extend to close and fill the opted for area.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000