Using Solid Edge Printer And ST8

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Matt,

Two questions: 1st. How to hock up to SE printer and or a tutorial on how to use. I show it in my printer file but cannot use.

2nd; Is the ST8 available for student edition

 

Thanks 

Greg

2 REPLIES

Re: Using Solid Edge Printer And ST8

Esteemed Contributor
Esteemed Contributor

PO_LC wrote:

How to hock up to SE printer and or a tutorial on how to use. I show it in my printer file but cannot use.

 


I presume you are talking about the Solid Edge Velocity PS Printer?....this creates a ".PRN" file, this is basically like machining code, that tells a printer what to do. 

 

From the Solid Edge HELP file...

Saving Solid Edge documents to Adobe Acrobat PDF

A Solid Edge Velocity PS Printer 2.0 printer driver is installed automatically with Solid Edge and is used by the Save As command to generate an Adobe PDF document. The default settings are sufficient for this purpose. To adjust the default PDF output properties, see the Help topic, Change PDF printer properties.

 


PO_LC wrote:

Is the ST8 available for student edition

 


 

Yes, it is available.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Using Solid Edge Printer And ST8

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Sean,

Since This One Year SE Student Edition Expires This Month Sept., I Would Like To Install The ST8 Software Student Edition.

 

Thanks 

Greg