is sold edge avail for Macs?

Experimenter
Experimenter

Hello, my son is interested in downloading the student version of Solid Edge but we have a mac and I am wondering if there is a version for macs?  All I see in the system requirements is windows... help!

1 REPLY

Re: is sold edge avail for Macs?

MattJohnson_PG 2nd Gear
2nd Gear

SE will not install on the MAC OS.  There are users running SE on MACs however.  It is my understanding that you need a "Boot Camp" like software that allows you to boot the machine into either the Apple OS or a Windows environment.  Once booted in the Windows environment you can install and run SE...

 

REF: https://support.apple.com/en-gb/HT201468

 

Good luck.

 

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.6