problems in frame environment

N/A
i am trying to solve a tutorial. when I try to convert a wire frame into 3d, it just not comes up to what it must be. i use square frame from the library.
i have attached a picture. to the right is what it actually should be and to the left is what it becomes.
need help
thanks.
2 REPLIES

Re: problems in frame environment

Valued Contributor
Valued Contributor
Looks like the sketch is too small. Are you using the correct unit of measurement?

Re: problems in frame environment

N/A
thanks rogerreid. That helped. the sketch was small as compared to frame cross section and i made a custom one. now there is another problem. in the frame structure, the frames overlap at the ends. in solid works, we can trim the profile. do i have any such option in solid edge?