Cancel
Showing results for 
Search instead for 
Did you mean: 

Watson_FishingReel_Keyshot_9 resized.jpg

A type of fishing reel known as a baitcasting reel has a handle with several gears linked together to turn the main spool. The system of gears also turns a bar at the top of the reel known as the "worm gear" which allows the pin at the top of the black line guide to move along the bar and keep the line from building up at one point on the spool. 

Baitcasting Fishing Reel

Dreamer

Watson_FishingReel_Keyshot_9 resized.jpg

A type of fishing reel known as a baitcasting reel has a handle with several gears linked together to turn the main spool. The system of gears also turns a bar at the top of the reel known as the "worm gear" which allows the pin at the top of the black line guide to move along the bar and keep the line from building up at one point on the spool.