Cancel
Showing results for 
Search instead for 
Did you mean: 

The new is here! This modern electronic device is the Game Cube 2. The newer version of the Game Cube now provides wireless controls with up to four controls at the same time. The 149mm x 160mm x 45mm device is now thinner and lighter than ever. This newer version also provides a 89mmx 102mm LCD TV screen display optional to use. Video game are now accessible from the Game Cube store rather than buying an actual CD or cassette. Taking gaming to a new level. This project was made in the University of Texas of Rio Grande Valley. 

Game Cube 2

Dreamer

The new is here! This modern electronic device is the Game Cube 2. The newer version of the Game Cube now provides wireless controls with up to four controls at the same time. The 149mm x 160mm x 45mm device is now thinner and lighter than ever. This newer version also provides a 89mmx 102mm LCD TV screen display optional to use. Video game are now accessible from the Game Cube store rather than buying an actual CD or cassette. Taking gaming to a new level. This project was made in the University of Texas of Rio Grande Valley.