Cancel
Showing results for 
Search instead for 
Did you mean: 

FishingReel.jpg

A team of five members from Michigan State University did a final project in their Graphic communications class. Four of us our mechanical engineers while one is an applied engineer. We are all currently sophomores. Our NX project is a fishing pole reel we designed each part and assembled it on NX. The motion of the reel is when you push the button down it allows it to hit the spring letting loose one of the bottom housing. This motion is to allow the line to be let loose so you can cast it. Another motion is being able to spin the handle which reels in the line.

 

info:

MSU - ME280 class

Professor: Kathy Stevenson (kstevens@msu.edu)

Team 5

 

The REEL deal

Dreamer

FishingReel.jpg

A team of five members from Michigan State University did a final project in their Graphic communications class. Four of us our mechanical engineers while one is an applied engineer. We are all currently sophomores. Our NX project is a fishing pole reel we designed each part and assembled it on NX. The motion of the reel is when you push the button down it allows it to hit the spring letting loose one of the bottom housing. This motion is to allow the line to be let loose so you can cast it. Another motion is being able to spin the handle which reels in the line.

 

info:

MSU - ME280 class

Professor: Kathy Stevenson (kstevens@msu.edu)

Team 5