Cancel
Showing results for 
Search instead for 
Did you mean: 

In the picture drawn on the laptop and the process of rendering images in the Siemens NX program. Apply multiple backgrounds to bargain realism.

Rendering is the process of generating an image from a 2D or 3D model (or models in what collectively could be called a scene file) by means of computer programs. Also, the results of such a model can be called a rendering. A scene file contains objects in a strictly defined language or data structure; it would contain geometry, viewpoint, texture, lighting, and shadow information as a description of the virtual scene. The term "rendering" may be by analogy with an "artist's rendering" of a scene. Though the technical details of rendering methods vary, the general challenges to overcome in producing a 2D image from a 3D representation stored in a scene file are outlined as the graphics pipeline along a rendering device, such as a GPU. A GPU is a purpose-built device able to assist a CPU in performing complex rendering calculations. If a scene is to look relatively realistic and predictable under virtual lighting, the rendering software should solve the rendering equation. The rendering equation doesn't account for all lighting phenomena, but is a general lighting model for computer-generated imagery. 'Rendering' is also used to describe the process of calculating effects in a video editing program to produce final video output.laptop 1.jpglaptop in work roomlaptop 2.jpglaptop and cappuccinolaptop.jpglaptop render

The process of rendering. Laptop

Visionary

In the picture drawn on the laptop and the process of rendering images in the Siemens NX program. Apply multiple backgrounds to bargain realism.

Rendering is the process of generating an image from a 2D or 3D model (or models in what collectively could be called a scene file) by means of computer programs. Also, the results of such a model can be called a rendering. A scene file contains objects in a strictly defined language or data structure; it would contain geometry, viewpoint, texture, lighting, and shadow information as a description of the virtual scene. The term "rendering" may be by analogy with an "artist's rendering" of a scene. Though the technical details of rendering methods vary, the general challenges to overcome in producing a 2D image from a 3D representation stored in a scene file are outlined as the graphics pipeline along a rendering device, such as a GPU. A GPU is a purpose-built device able to assist a CPU in performing complex rendering calculations. If a scene is to look relatively realistic and predictable under virtual lighting, the rendering software should solve the rendering equation. The rendering equation doesn't account for all lighting phenomena, but is a general lighting model for computer-generated imagery. 'Rendering' is also used to describe the process of calculating effects in a video editing program to produce final video output.laptop 1.jpglaptop in work roomlaptop 2.jpglaptop and cappuccinolaptop.jpglaptop render

Comments
Dreamer

beautiful