Cancel
Showing results for 
Search instead for 
Did you mean: 

Student Design Contest

  • I have modelled the Omega 'Alaska Project' watch as part of a visualisation module within my course, the watch is exciting as it is based on the watch that Omega first made to send to space with the apollo 11 mission to the moon in 1969,which featured a titanium case and white dials to deal with the extreme temperature variations of outer space. In the end the alaska project watch never made it into space however they did created the consumer edition to commermorate the first watches produced, this watch features more stylistic design elements while retaining original features like the case and the dial. The modelling for the module was undertaken in my first year at Loughborough University studying Product Design Engineering. All the 3D components were made in NX 11, the decals were produced in adobe Illustrator and the images were also rendered within NX 11's ray traced studio. The images then have post editing in photoshop afterwards to add vibrancy to the images.

     

    In the first picture the book and pencils were also modelled by me and I also produced the decals for them in illustrator.

     

    TABLEJPG.jpgUsing a HDRI imge for the backgroundMACROJPG.jpgClose up shot of the rear of the watch featuring decals and Omega Seamaster logo that was modelled to add correct look of depthENSEMBLEJPG.jpgWhite space render of the watch displaying it with and without the outercase

    I tried to keep a high level of detail and a focus on lighting and the use of the depth of field within NX11 to produce the most realistic renders possible and am proud of the outcome. I enjoyed the whole process of modelling and rendering and look forward to my continued use of NX11 as a modelling package.

     

    If i were to repeat the whole process I would alter the paint texture on the tachymetre as it is a little to sharp, I would also add an  edge blend to the seamaster logo on the macro shot, I wasn't able to this as the area was too small and many of  the edges overlapped so I would possibly attempt to offset the sketch to give myself an area to edge blend, however this project had time constraints so I am happy with what I produced. 

    2019-June Winner - Watch This Space

    Enthusiast

    I have modelled the Omega 'Alaska Project' watch as part of a visualisation module within my course, the watch is exciting as it is based on the watch that Omega first made to send to space with the apollo 11 mission to the moon in 1969,which featured a titanium case and white dials to deal with the extreme temperature variations of outer space. In the end the alaska project watch never made it into space however they did created the consumer edition to commermorate the first watches produced, this watch features more stylistic design elements while retaining original features like the case and the dial. The modelling for the module was undertaken in my first year at Loughborough University studying Product Design Engineering. All the 3D components were made in NX 11, the decals were produced in adobe Illustrator and the images were also rendered within NX 11's ray traced studio. The images then have post editing in photoshop afterwards to add vibrancy to the images.

     

    In the first picture the book and pencils were also modelled by me and I also produced the decals for them in illustrator.

     

    TABLEJPG.jpgUsing a HDRI imge for the backgroundMACROJPG.jpgClose up shot of the rear of the watch featuring decals and Omega Seamaster logo that was modelled to add correct look of depthENSEMBLEJPG.jpgWhite space render of the watch displaying it with and without the outercase

    I tried to keep a high level of detail and a focus on lighting and the use of the depth of field within NX11 to produce the most realistic renders possible and am proud of the outcome. I enjoyed the whole process of modelling and rendering and look forward to my continued use of NX11 as a modelling package.

     

    If i were to repeat the whole process I would alter the paint texture on the tachymetre as it is a little to sharp, I would also add an  edge blend to the seamaster logo on the macro shot, I wasn't able to this as the area was too small and many of  the edges overlapped so I would possibly attempt to offset the sketch to give myself an area to edge blend, however this project had time constraints so I am happy with what I produced. 

  • My name is Danielle, I have just finished my first year of Product Design Engineering, BEng, at Loughborough University. 

    As a part of a visualisation module, I created a model of a Harken self-tailoring winch used on sailing yachts. The winch enables large quantities of tension to be applied to halyards that would not otherwise be possible through manpower. This is done through the friction applied to the gears and bearings within the device, with the NX software I was able to include these detailed parts and constraint them to the final model assembly. 
    The main focus of the project was to create a model of a product that was a representation of the original object. This was done through the use of lighting and shadow effect in the RayTrace studio of the NX software. HDR images were used for the mirrored environment effect on surfaces meaning when the final render was exported onto a visual scene the model slotted in seamlessly. 
    I feel I have embellished my NX skill base throughout this project which I look forward to using again in future tasks.

    3. Final Winch- HDR.jpgFinal render of winch (NX)

    5. Final Winch- ropes.jpgAction shot of the winch (NX & Photoshop [background image from google])

    2018 September Winner-Harken Sailing Winch

    Theorist

    My name is Danielle, I have just finished my first year of Product Design Engineering, BEng, at Loughborough University. 

    As a part of a visualisation module, I created a model of a Harken self-tailoring winch used on sailing yachts. The winch enables large quantities of tension to be applied to halyards that would not otherwise be possible through manpower. This is done through the friction applied to the gears and bearings within the device, with the NX software I was able to include these detailed parts and constraint them to the final model assembly. 
    The main focus of the project was to create a model of a product that was a representation of the original object. This was done through the use of lighting and shadow effect in the RayTrace studio of the NX software. HDR images were used for the mirrored environment effect on surfaces meaning when the final render was exported onto a visual scene the model slotted in seamlessly. 
    I feel I have embellished my NX skill base throughout this project which I look forward to using again in future tasks.

    3. Final Winch- HDR.jpgFinal render of winch (NX)

    5. Final Winch- ropes.jpgAction shot of the winch (NX & Photoshop [background image from google])

  • My name is amartei , a mechanical engineering student of the Kwame Nkrumah University of Science and Technology.I decided to attempt the problem faced by most industries in powering electronic equipment on rotating shafts without wearing of rotating and stationary parts and also providing continuous uninterrupted power supply to equipment mounted on the shaft to prevent downtime in equipment operation. I enjoyed the theme for the project whilst i created various part components in nx. I decicided to use a detachable belt drive which linked the rotating shaft to a generator for continuous power supply where the power generated is conducted through an electrolyte solution to the rotating equipment mounted on the shaft.This idea remains only  as a concept. 

     

    assembly 1.jpgassembly 2.jpgassembly.jpg

    saved.jpg

     

    Powering Electronic Equipment on Rotating Shaft

    Visionary

    My name is amartei , a mechanical engineering student of the Kwame Nkrumah University of Science and Technology.I decided to attempt the problem faced by most industries in powering electronic equipment on rotating shafts without wearing of rotating and stationary parts and also providing continuous uninterrupted power supply to equipment mounted on the shaft to prevent downtime in equipment operation. I enjoyed the theme for the project whilst i created various part components in nx. I decicided to use a detachable belt drive which linked the rotating shaft to a generator for continuous power supply where the power generated is conducted through an electrolyte solution to the rotating equipment mounted on the shaft.This idea remains only  as a concept. 

     

    assembly 1.jpgassembly 2.jpgassembly.jpg

    saved.jpg

     

    • NX
  • Hello! My name is Maria Yureva. I'm a 4th year student of Belgorod State Technological University named after V.G. Shukhov (Computer Technologies in Mechanical Engineering of Building Material Industry).

    I have always wondered why in the building materials industry is relatively little space is given to machine for lifting? Flipped through magazines CAD, look at the huge posters in the design lab - all entirely deeply special equipment used only in the building materials industry. But there is also a machine for lifting, without which virtually every enterprise absolutely any industry can not do! Such machines and relates elevator LGNS-260, which lifts the material in the vertical direction by means of deep bucket. And I began my acquaintance with the elevator that's how.

    As a student-designer I needed to find machine drawings, which I will design. And began to search the Internet, trips to factories, but significant results to no avail: in the best case, you can find the drawings only a general form without detailing. Then I went to an old and good friend in another city who have a lot of other friends, without a drawing for the soul, and with ardent hope in your heart. And a miracle happened! The drawings came to me in full, and even in electronic form. Happy and satisfied, I went home.

    First, the elevator I was even more frightened by their size, and it was very interesting - if I have time to build and collect all in such a short time? However, as the saying goes, "the eyes to fear, but the hands are doing." Having examined the drawings and specifications, I walked into the Teamcenter, create a product structure established in Annex "Structure Manager" and opened NX.

    Teamcenter - a suite of scalable software solutions to support the life cycle of products that are based on an open PLM platform. Teamcenter enables you to communicate to all participants create a product intelligently managing, maintaining, distributing and enhancing intellectual property companies. In addition to work on the elevator it was used not just Teamcenter, and the SSP - a prototype of the standard solutions. This is a prepared set of settings and methods, providing the implementation of the most popular problems that can be solved in Teamcenter and NX systems. Comfortable and functional open the system settings did work on the elevator fast and productive, so that the diploma, with all its immense amount of detail, was ready on time.

    At all stages of product development teachers supervised the creation of the machine. top-level nodes selectively passed through the approval process. And now finally designed the elevator emblazoned on a realistic image of my diploma.

    elevator_1re.pngelevator_2re.png

    22-06-2016 9-24-26.pngCAE analysis of bearing partelevator_3.pngelevator_4.png

    Elevator LGNS-260

    Visionary

    Hello! My name is Maria Yureva. I'm a 4th year student of Belgorod State Technological University named after V.G. Shukhov (Computer Technologies in Mechanical Engineering of Building Material Industry).

    I have always wondered why in the building materials industry is relatively little space is given to machine for lifting? Flipped through magazines CAD, look at the huge posters in the design lab - all entirely deeply special equipment used only in the building materials industry. But there is also a machine for lifting, without which virtually every enterprise absolutely any industry can not do! Such machines and relates elevator LGNS-260, which lifts the material in the vertical direction by means of deep bucket. And I began my acquaintance with the elevator that's how.

    As a student-designer I needed to find machine drawings, which I will design. And began to search the Internet, trips to factories, but significant results to no avail: in the best case, you can find the drawings only a general form without detailing. Then I went to an old and good friend in another city who have a lot of other friends, without a drawing for the soul, and with ardent hope in your heart. And a miracle happened! The drawings came to me in full, and even in electronic form. Happy and satisfied, I went home.

    First, the elevator I was even more frightened by their size, and it was very interesting - if I have time to build and collect all in such a short time? However, as the saying goes, "the eyes to fear, but the hands are doing." Having examined the drawings and specifications, I walked into the Teamcenter, create a product structure established in Annex "Structure Manager" and opened NX.

    Teamcenter - a suite of scalable software solutions to support the life cycle of products that are based on an open PLM platform. Teamcenter enables you to communicate to all participants create a product intelligently managing, maintaining, distributing and enhancing intellectual property companies. In addition to work on the elevator it was used not just Teamcenter, and the SSP - a prototype of the standard solutions. This is a prepared set of settings and methods, providing the implementation of the most popular problems that can be solved in Teamcenter and NX systems. Comfortable and functional open the system settings did work on the elevator fast and productive, so that the diploma, with all its immense amount of detail, was ready on time.

    At all stages of product development teachers supervised the creation of the machine. top-level nodes selectively passed through the approval process. And now finally designed the elevator emblazoned on a realistic image of my diploma.

    elevator_1re.pngelevator_2re.png

    22-06-2016 9-24-26.pngCAE analysis of bearing partelevator_3.pngelevator_4.png

  • 3-1.jpg

    A blend of Siemens NX and Adobe Photoshop.

    Bialetti Coffee Maker Render -2018 July Winner

    Enthusiast

    3-1.jpg

    A blend of Siemens NX and Adobe Photoshop.

  • My name is Kai Mendes; I am a 1st Year Product Design Engineering student studying at Loughborough University in England. As part of our course, we were required to take an object (or in my case, several) to model and render within NX 11. I created the Nintendo Switch, controllers and accessories, including the entire room, rendered fully within NX using Ray Traced Studio without the use of any external programs such as Photoshop.

     

    KRMendes - Nintendo Switch Render Competition Entry LOW QUALITY.jpgNintendo Switch Controller, Console, Accessories and Room, Fully Rendered (Please note: this is a .JPG of the original .TIF so that the image could be small enough to be embedded into this post. Please find the original, high quality .TIF at the specified resolution attached to this post for judging).

    I decided to render the newest gaming console from Nintendo (creators of famed gaming icons such as Mario, Pokémon and Zelda) the Nintendo Switch; a hybrid between a traditional home console and a portable one, the Nintendo Switch allows you to dock the main unit to play in a living room environment, or remove it and attach the detachable controllers (called Joy-Cons) via rails on the side of the console.

     

    The Joy-Cons can also be attached to a grip (as seen in the centre of the main image), attached to wrist straps for games that require movement of the controllers (as seen to the left of the image), or be used freely without a grip or straps (as seen to the right of the image). I also rendered various accessories, such as game cases (to the right), two figures of popular Nintendo characters that can be used with the console via NFC communication with the controllers to gain in-game rewards (to the left), as well as the dock (under the television). The Nintendo Switch and the various accessories I modelled can be seen within Supplementary Image #3, all of which are annotated for easy reference.

     

    For this specific render, I also created the entire room, from the coffee table the controllers sit on, to the walls, to the TV as well as the chair. To gain complex lighting and shadows, I included a window (which can’t be seen in this render, but can be seen within Supplementary Image #2) which has a light filtering through it, as well as using a HDRI image. I also created a backlit television using NX’s material options, by using the “Area Light” material and a decal sticker with its reflectivity set to glass, which created a bright, realistic screen, which is also reflected in the glass of the coffee table due to the backlight.

     

    I had to use a range of NX’s functions to create all the object seen within the image; from basics such as the Extrude and Revolve commands, to projecting sketches, transforming bodies, using the X-Form command, using Studio Splines and Tubes for the wrist straps, Decal Stickers for the logos, and various complex assemblies; creating a full set of objects that were as true to life as possible required a deep understanding on my part of the various functions NX is capable of.

     

    I aimed to fully use the complexity of NX’s rendering tools, which has allowed me to gain effects that using a simple 2D background image wouldn’t have created, and without the use of external programs; from the lights, to the various shadows, to the various reflections: the reflection of room on the TV; the reflection of the TV screen on the glass of the coffee table; the reflection of the blue Joy-Con in the controller grip; as seen within Supplementary Image #1; everything was fully created using NX and Ray Traced Studio.

     

    Supplementary Images:

     

    KRMendes - Supplementary Image 1.pngSupplementary Image #1 - View of the models and environment used to fully render the final image.KRMendes - Supplementary Image 2.pngSupplementary Image #2 - View of the entire room environment. The detail within the environment allows for complex lighting arrangements and fine details.KRMendes - Supplementary Image 3.pngSupplementary Image #3 - (1,2,8,10 = Nintendo Switch Joy-Con Controller) (3,4 = NFC Figures) (5 = Controller Grip) (6,13 = Game Cases) (7 = Controller Wrist Straps) (9 = Nintendo Switch Console Unit) (11 = Game Cartridges) (12 = Nintendo Switch Dock)

    Nintendo Switch Controllers, Console, Accessories and Room, Fully Rendered

    Enthusiast

    My name is Kai Mendes; I am a 1st Year Product Design Engineering student studying at Loughborough University in England. As part of our course, we were required to take an object (or in my case, several) to model and render within NX 11. I created the Nintendo Switch, controllers and accessories, including the entire room, rendered fully within NX using Ray Traced Studio without the use of any external programs such as Photoshop.

     

    KRMendes - Nintendo Switch Render Competition Entry LOW QUALITY.jpgNintendo Switch Controller, Console, Accessories and Room, Fully Rendered (Please note: this is a .JPG of the original .TIF so that the image could be small enough to be embedded into this post. Please find the original, high quality .TIF at the specified resolution attached to this post for judging).

    I decided to render the newest gaming console from Nintendo (creators of famed gaming icons such as Mario, Pokémon and Zelda) the Nintendo Switch; a hybrid between a traditional home console and a portable one, the Nintendo Switch allows you to dock the main unit to play in a living room environment, or remove it and attach the detachable controllers (called Joy-Cons) via rails on the side of the console.

     

    The Joy-Cons can also be attached to a grip (as seen in the centre of the main image), attached to wrist straps for games that require movement of the controllers (as seen to the left of the image), or be used freely without a grip or straps (as seen to the right of the image). I also rendered various accessories, such as game cases (to the right), two figures of popular Nintendo characters that can be used with the console via NFC communication with the controllers to gain in-game rewards (to the left), as well as the dock (under the television). The Nintendo Switch and the various accessories I modelled can be seen within Supplementary Image #3, all of which are annotated for easy reference.

     

    For this specific render, I also created the entire room, from the coffee table the controllers sit on, to the walls, to the TV as well as the chair. To gain complex lighting and shadows, I included a window (which can’t be seen in this render, but can be seen within Supplementary Image #2) which has a light filtering through it, as well as using a HDRI image. I also created a backlit television using NX’s material options, by using the “Area Light” material and a decal sticker with its reflectivity set to glass, which created a bright, realistic screen, which is also reflected in the glass of the coffee table due to the backlight.

     

    I had to use a range of NX’s functions to create all the object seen within the image; from basics such as the Extrude and Revolve commands, to projecting sketches, transforming bodies, using the X-Form command, using Studio Splines and Tubes for the wrist straps, Decal Stickers for the logos, and various complex assemblies; creating a full set of objects that were as true to life as possible required a deep understanding on my part of the various functions NX is capable of.

     

    I aimed to fully use the complexity of NX’s rendering tools, which has allowed me to gain effects that using a simple 2D background image wouldn’t have created, and without the use of external programs; from the lights, to the various shadows, to the various reflections: the reflection of room on the TV; the reflection of the TV screen on the glass of the coffee table; the reflection of the blue Joy-Con in the controller grip; as seen within Supplementary Image #1; everything was fully created using NX and Ray Traced Studio.

     

    Supplementary Images:

     

    KRMendes - Supplementary Image 1.pngSupplementary Image #1 - View of the models and environment used to fully render the final image.KRMendes - Supplementary Image 2.pngSupplementary Image #2 - View of the entire room environment. The detail within the environment allows for complex lighting arrangements and fine details.KRMendes - Supplementary Image 3.pngSupplementary Image #3 - (1,2,8,10 = Nintendo Switch Joy-Con Controller) (3,4 = NFC Figures) (5 = Controller Grip) (6,13 = Game Cases) (7 = Controller Wrist Straps) (9 = Nintendo Switch Console Unit) (11 = Game Cartridges) (12 = Nintendo Switch Dock)

    • NX
  •  

    Giving an iconic design new life.

     

    This is a shell of one of the old hitachi boom boxes from the 80's.

    It can run off batteries or the mains, the former leading to the iconic image of youths walking around with these speakers slung over one shoulder blasting out the latest tunes. 

     

    I modelled and rendered this image in NX 10, creating my own decals in photoshop, even the radio band display had to be custom made to be accurate to the true design. The detail dosn't stop there, fine details such as the tape spools, button dimples, and tuner dial grip are true to life.

     

    Institution: Loughborough university

    Degree: Sport Technologycompress.pngMy Image (compressed)high_q_7.pngClose up (compressed)top_compress.pngA view form up top (compressed)vintage-hitachi-3d-bass-super-woofer_360_7a99ae10edcc8d07a09ef649c248bca6.jpgThe product

    Hitachi 3D Bass Super Woofer -July 2017 Winner

    Enthusiast

     

    Giving an iconic design new life.

     

    This is a shell of one of the old hitachi boom boxes from the 80's.

    It can run off batteries or the mains, the former leading to the iconic image of youths walking around with these speakers slung over one shoulder blasting out the latest tunes. 

     

    I modelled and rendered this image in NX 10, creating my own decals in photoshop, even the radio band display had to be custom made to be accurate to the true design. The detail dosn't stop there, fine details such as the tape spools, button dimples, and tuner dial grip are true to life.

     

    Institution: Loughborough university

    Degree: Sport Technologycompress.pngMy Image (compressed)high_q_7.pngClose up (compressed)top_compress.pngA view form up top (compressed)vintage-hitachi-3d-bass-super-woofer_360_7a99ae10edcc8d07a09ef649c248bca6.jpgThe product

  • Loughborough University 1st year  Product Design Engineering Student

    2017 Sept Winner - Bodum Cafetiere

    Enthusiast

    Loughborough University 1st year  Product Design Engineering Student

  • For my first-year visualisation module at Loughborough University, I chose to model and render my pocket watch. 

    After producing dimensioned drawings of the watch I set about modelling each part of the main body individually and then assembled them in a master assembly file. Through utilizing a wide range of functions including revolving, patterning and curve projection, I full modelled not only the outside form of the watch but also the internal workings. I took care that the gears, springs and screws all fully aligned and interlocked as to be as accurate to the watch as possible.

    I added small blends to make various edges of components "pop" in the light and modified facet settings to improve the quality of my forms. After this, I set about rendering my design by selecting the default materials and then editing and modifying the advanced settings, for example by adding extra texture layers and changing reflectivity. I then spent time finding a range of lighting settings and setups ranging from dark room spotlights to bright studio lighting to create a range of visualisations. Through assembly constraints, I also made the model fully movable which allowed me to open and close the casing, rotate the clock hands and move the top ring. 

    I was very pleased with the final outcome and my range of visualisations and continue to refine my CAD skills between university projects. 1.jpg4.jpg5.jpg

    2018 October Winner - Antique Pocket Watch

    Theorist

    For my first-year visualisation module at Loughborough University, I chose to model and render my pocket watch. 

    After producing dimensioned drawings of the watch I set about modelling each part of the main body individually and then assembled them in a master assembly file. Through utilizing a wide range of functions including revolving, patterning and curve projection, I full modelled not only the outside form of the watch but also the internal workings. I took care that the gears, springs and screws all fully aligned and interlocked as to be as accurate to the watch as possible.

    I added small blends to make various edges of components "pop" in the light and modified facet settings to improve the quality of my forms. After this, I set about rendering my design by selecting the default materials and then editing and modifying the advanced settings, for example by adding extra texture layers and changing reflectivity. I then spent time finding a range of lighting settings and setups ranging from dark room spotlights to bright studio lighting to create a range of visualisations. Through assembly constraints, I also made the model fully movable which allowed me to open and close the casing, rotate the clock hands and move the top ring. 

    I was very pleased with the final outcome and my range of visualisations and continue to refine my CAD skills between university projects. 1.jpg4.jpg5.jpg

  • As part of my 1st year visualisation module at Loughborough University I was asked to produce images of my own choice effectively.

     

    The Duronic Ecohand AM/FM Radio was modelled and put together using the combination of NX 11 and Adobe Photoshop.

     

    The primary aim of the project was to create the perfect representation of the product chosen. By using the functions like environment, lighting and shadow with an appropriate background, realistic images were created using the Ray Traced Studio.

     

    Overall, creating the images was definitely challenging as an NX beginner but was also a fun experience as I have learnt a lot throughout this project.

     

    submission.jpg

    Duronic Ecohand AM/FM Radio

    Theorist

    As part of my 1st year visualisation module at Loughborough University I was asked to produce images of my own choice effectively.

     

    The Duronic Ecohand AM/FM Radio was modelled and put together using the combination of NX 11 and Adobe Photoshop.

     

    The primary aim of the project was to create the perfect representation of the product chosen. By using the functions like environment, lighting and shadow with an appropriate background, realistic images were created using the Ray Traced Studio.

     

    Overall, creating the images was definitely challenging as an NX beginner but was also a fun experience as I have learnt a lot throughout this project.

     

    submission.jpg

    • NX
  • In the lexicon of motor-fans it appeared the word "Dnepr". So called new road bike with a sidecar, created in Kiev Motorcycle Plant. In accordance with the methodology adopted by the people of Kiev have divided the development process of the machine in two steps. The first - is the construction, testing, debugging and manufacturing engine - more powerful and more economical. It is installed on the vehicle-part model is now manufactured. The second - the development of advanced vehicle-part, which is mounted already mastered, but a forced induction engine

    The engine crankshaft MT8 non-stackable (cast) of ductile iron. Lower head split connecting rods rotate on the sliding bearings (bushings), borrowed from the engine "Moskvich-408". Replacement pads are relatively simple, it requires on average after 50 thousand kilometers. Plain bearings are very demanding on the oil clean, so it is purified in a centrifuge mounted on the front of the crankshaft journal. Recall: the engine 750m K-rod bearings of the crankshaft are lubricated by feeding flowing from the jet pump. In MT8 oil supplied to these nodes at a higher pressure (2-4 atm.) With a pre-treatment in a centrifuge. This greatly reduces the wear of the friction surfaces and increases component life. Even when pressing on the foot control with a powerful pump to deliver oil to the lubrication points, making it easier to start the engine. The original pressure reducing valve bypass oil, preventing it is not mixed with purified centrifuge.Dnepr Motorcycle engine.jpgDnepr Motorcycle engineDnepr Motorcycle engine 1.jpgDnepr Motorcycle engine (cylinder not shown)Dnepr Motorcycle engine 2.jpgDnepr Motorcycle engineDnepr Motorcycle engine 3.jpgDnepr Motorcycle engine (Corps not shown)

    Dnepr Motorcycle engine-May Winner

    Visionary

    In the lexicon of motor-fans it appeared the word "Dnepr". So called new road bike with a sidecar, created in Kiev Motorcycle Plant. In accordance with the methodology adopted by the people of Kiev have divided the development process of the machine in two steps. The first - is the construction, testing, debugging and manufacturing engine - more powerful and more economical. It is installed on the vehicle-part model is now manufactured. The second - the development of advanced vehicle-part, which is mounted already mastered, but a forced induction engine

    The engine crankshaft MT8 non-stackable (cast) of ductile iron. Lower head split connecting rods rotate on the sliding bearings (bushings), borrowed from the engine "Moskvich-408". Replacement pads are relatively simple, it requires on average after 50 thousand kilometers. Plain bearings are very demanding on the oil clean, so it is purified in a centrifuge mounted on the front of the crankshaft journal. Recall: the engine 750m K-rod bearings of the crankshaft are lubricated by feeding flowing from the jet pump. In MT8 oil supplied to these nodes at a higher pressure (2-4 atm.) With a pre-treatment in a centrifuge. This greatly reduces the wear of the friction surfaces and increases component life. Even when pressing on the foot control with a powerful pump to deliver oil to the lubrication points, making it easier to start the engine. The original pressure reducing valve bypass oil, preventing it is not mixed with purified centrifuge.Dnepr Motorcycle engine.jpgDnepr Motorcycle engineDnepr Motorcycle engine 1.jpgDnepr Motorcycle engine (cylinder not shown)Dnepr Motorcycle engine 2.jpgDnepr Motorcycle engineDnepr Motorcycle engine 3.jpgDnepr Motorcycle engine (Corps not shown)

    • NX
  • I designed a unique pair of skis based on the general shape of contour skis and several ski bindings. In the image is one ski, set on a wood deck among the mountains. The ski has a blizzard logo on the front and an image of mountains on the side of the rear part of the ski bindings, as a potential company logo. The toe cup (blue), heel leaver (dark grey blue), heel cup (blue) and brake (silver, dark grey blue, black) are all movable, to allow the ski to be pictured in a state of no-boot on the ski, and boot on the ski.

     

    This ski was made as part of a visualisation module, which is part of my 1st year Product Design Engineering degree at Loughborough University.Mount-Ski.jpg

    2018 August Winner - Mount-Ski

    Dreamer

    I designed a unique pair of skis based on the general shape of contour skis and several ski bindings. In the image is one ski, set on a wood deck among the mountains. The ski has a blizzard logo on the front and an image of mountains on the side of the rear part of the ski bindings, as a potential company logo. The toe cup (blue), heel leaver (dark grey blue), heel cup (blue) and brake (silver, dark grey blue, black) are all movable, to allow the ski to be pictured in a state of no-boot on the ski, and boot on the ski.

     

    This ski was made as part of a visualisation module, which is part of my 1st year Product Design Engineering degree at Loughborough University.Mount-Ski.jpg

  • The new is here! This modern electronic device is the Game Cube 2. The newer version of the Game Cube now provides wireless controls with up to four controls at the same time. The 149mm x 160mm x 45mm device is now thinner and lighter than ever. This newer version also provides a 89mmx 102mm LCD TV screen display optional to use. Video game are now accessible from the Game Cube store rather than buying an actual CD or cassette. Taking gaming to a new level. This project was made in the University of Texas of Rio Grande Valley. 

    Game Cube 2

    Dreamer

    The new is here! This modern electronic device is the Game Cube 2. The newer version of the Game Cube now provides wireless controls with up to four controls at the same time. The 149mm x 160mm x 45mm device is now thinner and lighter than ever. This newer version also provides a 89mmx 102mm LCD TV screen display optional to use. Video game are now accessible from the Game Cube store rather than buying an actual CD or cassette. Taking gaming to a new level. This project was made in the University of Texas of Rio Grande Valley. 

    • NX
  • Greetings, my name is Nikita Bogdanov, I am a fourth year student of the Belgorod State Technological University named after Shukhov, I study at the Faculty of "Mechanical equipment" my specialty – is Mechanical Engineer and my specialization – is to use computer aided design systems in design of mechanical equipment, and I want to introduce you the topic of my qualifying, graduate work, which I will defend this year. Equipment that is used in my project - the rotary kiln for cement production.  Kiln - is the main process unit of any cement plant. And It is very important because klinker and cement quality depends on correct performance of this equipment.

     

    As the construction of the rotary kiln is very complicated, this qualification work was shared between 3 students with my uni-comrades (Konstantin Vavilov and Mikhail Shvec). I believe, working on this project will give us essential experience  that will us help in future professional activities. Though, each of us creates  different assembly units of one machine, it is very important to avoid mistakes in this process. The final result of our qualifying project depends on our well-coordinated teamwork.

     

    We began to work on this project ten  months ago, during a summer practice at the university, with the analysis of the equipment industry of building materials.   I carried out market analysis of this equipment and found products of leading Kiln manufacturers (Flsmidth, KHD Humboldt Wedag, ThyssenKrupp,  and others). We have analyzed advantages and disadvantages of presented examples. Kilns are different in the diameter and length, number of supports, design of the sealing device, the type of the support bearing and etc. Generally, Kilns have a number of drawbacks: the heat loss due to imperfect sealing device, the complexity of the repair, wear of tire and ring gear.

     

    Manufacturers produce both 2-base kiln (which is considered to be more progressive solution, because of lower metal consumption) and 3-base-kiln (it is classical solution and that is why it is quite easy to operate). Therefore, We proposed possible solutions of these problems, approved by university professors staff, aimed to improve disadvantages of the kiln.

    Then we formulated the goal of our project:

    -Create a unified digital model, which allows to control the structure of equipment and have two different types of kiln- 2-base-kiln and 3-base-kiln 4x60m.

    -Conduct improvement of assembly units of both kilns s in order to increase the efficiency of the kilns  based of patent search.

    We use NX, and Teamcenter  to work on our graduation project. Opportunities of the software NX and Teamcenter allow us to make all what we have planned before. In unified digital model, we will create two options quite different in design kilns: 2-base-kiln and 3-base-kiln. While these kilns are of equal size, but they have different designs:

    2-base-kiln have a friction drive, self-adjustable roller support

    3-base-kiln have a gear drive, tangential, tangential mounting of the tyre.

    These kilns have a different steel shells (order and number of shells)

    And both of them have the same supporting bearing, sealing and hydraulic thrust devices.

     

    After that, we developed the structure of our machine in the Teamcenter manager structure and divided the workload between each of us to have the implementation process of qualifying work more balanced. It is a very important, as the process of the structure development can be changed in extreme case. Here you can see assembly units and specification of our kiln made in Teamcenter structure manager:

    1)Rotary part of the 3 base-kiln, 2) Rotary part of the 2 base-kiln, 3) Ø400 Roller support of 3-base kiln , 4) Ø450 Roller support of 3-base kiln , 5) Ø400 Roller support of 2-base kiln,  6) Gearing drive, 7)Ring gear, 8) Under-Ring gear, 9) Friction drive, 10) Cold end seal, 11) Hot end seal, 12) Hydraulic Thrust Device.

     

    The finished components was revised by professors staff (technical control, compliance assessment, control of the project manager) with help of work process in Teamcenter. In case of mistakes, we discuss the problems with professors and improve parts and components until it finally approved, without the possibility of further changes.

     

    Our project contains 12435 parts, including 552 unique parts.

     

    In our work we also use a SSP -  prototype of the standard solutions. This is open data-model (prepared set of settings and methods) which Siemens PLM software deliver to users all over the world. In our work SSP helped us to adapt work of NX and Teamcenter to conditons of russian stantards - GOST and ESKD. Moreover SSP had great functional affecting process of creating drawings like automatic filling of labels on sheets. This features helped us a lot, and made process of implementation of our diploma work much more easy.

     

    Then, as part of the degree project we  developed design documentation on 2-base-kiln, conducted strength l conditions of the kiln body in CAE-Nastran  and made a set of working drawings.2 — копия.jpgrotary kilns

    3.jpgfriction drive5.jpgself-adjustable roller support

    3333.pngStructure manager with variants4444.pngStress analysis of rotary part

    Rotary kiln

    Enthusiast

    Greetings, my name is Nikita Bogdanov, I am a fourth year student of the Belgorod State Technological University named after Shukhov, I study at the Faculty of "Mechanical equipment" my specialty – is Mechanical Engineer and my specialization – is to use computer aided design systems in design of mechanical equipment, and I want to introduce you the topic of my qualifying, graduate work, which I will defend this year. Equipment that is used in my project - the rotary kiln for cement production.  Kiln - is the main process unit of any cement plant. And It is very important because klinker and cement quality depends on correct performance of this equipment.

     

    As the construction of the rotary kiln is very complicated, this qualification work was shared between 3 students with my uni-comrades (Konstantin Vavilov and Mikhail Shvec). I believe, working on this project will give us essential experience  that will us help in future professional activities. Though, each of us creates  different assembly units of one machine, it is very important to avoid mistakes in this process. The final result of our qualifying project depends on our well-coordinated teamwork.

     

    We began to work on this project ten  months ago, during a summer practice at the university, with the analysis of the equipment industry of building materials.   I carried out market analysis of this equipment and found products of leading Kiln manufacturers (Flsmidth, KHD Humboldt Wedag, ThyssenKrupp,  and others). We have analyzed advantages and disadvantages of presented examples. Kilns are different in the diameter and length, number of supports, design of the sealing device, the type of the support bearing and etc. Generally, Kilns have a number of drawbacks: the heat loss due to imperfect sealing device, the complexity of the repair, wear of tire and ring gear.

     

    Manufacturers produce both 2-base kiln (which is considered to be more progressive solution, because of lower metal consumption) and 3-base-kiln (it is classical solution and that is why it is quite easy to operate). Therefore, We proposed possible solutions of these problems, approved by university professors staff, aimed to improve disadvantages of the kiln.

    Then we formulated the goal of our project:

    -Create a unified digital model, which allows to control the structure of equipment and have two different types of kiln- 2-base-kiln and 3-base-kiln 4x60m.

    -Conduct improvement of assembly units of both kilns s in order to increase the efficiency of the kilns  based of patent search.

    We use NX, and Teamcenter  to work on our graduation project. Opportunities of the software NX and Teamcenter allow us to make all what we have planned before. In unified digital model, we will create two options quite different in design kilns: 2-base-kiln and 3-base-kiln. While these kilns are of equal size, but they have different designs:

    2-base-kiln have a friction drive, self-adjustable roller support

    3-base-kiln have a gear drive, tangential, tangential mounting of the tyre.

    These kilns have a different steel shells (order and number of shells)

    And both of them have the same supporting bearing, sealing and hydraulic thrust devices.

     

    After that, we developed the structure of our machine in the Teamcenter manager structure and divided the workload between each of us to have the implementation process of qualifying work more balanced. It is a very important, as the process of the structure development can be changed in extreme case. Here you can see assembly units and specification of our kiln made in Teamcenter structure manager:

    1)Rotary part of the 3 base-kiln, 2) Rotary part of the 2 base-kiln, 3) Ø400 Roller support of 3-base kiln , 4) Ø450 Roller support of 3-base kiln , 5) Ø400 Roller support of 2-base kiln,  6) Gearing drive, 7)Ring gear, 8) Under-Ring gear, 9) Friction drive, 10) Cold end seal, 11) Hot end seal, 12) Hydraulic Thrust Device.

     

    The finished components was revised by professors staff (technical control, compliance assessment, control of the project manager) with help of work process in Teamcenter. In case of mistakes, we discuss the problems with professors and improve parts and components until it finally approved, without the possibility of further changes.

     

    Our project contains 12435 parts, including 552 unique parts.

     

    In our work we also use a SSP -  prototype of the standard solutions. This is open data-model (prepared set of settings and methods) which Siemens PLM software deliver to users all over the world. In our work SSP helped us to adapt work of NX and Teamcenter to conditons of russian stantards - GOST and ESKD. Moreover SSP had great functional affecting process of creating drawings like automatic filling of labels on sheets. This features helped us a lot, and made process of implementation of our diploma work much more easy.

     

    Then, as part of the degree project we  developed design documentation on 2-base-kiln, conducted strength l conditions of the kiln body in CAE-Nastran  and made a set of working drawings.2 — копия.jpgrotary kilns

    3.jpgfriction drive5.jpgself-adjustable roller support

    3333.pngStructure manager with variants4444.pngStress analysis of rotary part

  • My name is Denis, I am studying at the National Aerospace University "HAI", specialties of rocket and space complexes. This paper would like fashin the full range of course design. Your attention is available aircraft class "air-air". Rocket R-24 сompleted the normal aerodynamic scheme with destabilizers located on homing housing. The missile can be equipped with semi-active radar homing (R-24R) or heat (R-24T). The size and position destabilizers are selected depending on the type of GOS thus to maintain constant torque characteristics of a rocket.
    The most noticeable external difference between the new missiles on the P-23 was the use of forward-swept wings with the back edge. Changed and interior layout, the number of sections was reduced from 8 to 5. The first compartment has traditionally been a seeker. Rod warhead with a blast radius of 10 m and a slam-actuator is moved into the third compartment.Air-Air Missile 1.jpgAir-Air MissileAir-Air Missile.jpgAir-Air Missile 2

    Solid engine PRD-287 forms a fourth compartment. The engine has an increased work time, provides greater range and flight speed of up to M = 3.5. engine igniter.jpgengine igniterRocket engine solid fuel.jpgRocket engine solid fuel

    In the fifth compartment around the flue elongated nozzle unit housed gas generators providing power steering gears.The engine nozzle.jpgThe engine nozzle

    The wing has a trapezoidal form in plan and with sharpened edges of the front and rear sides. Linked wing body consists of extruded sheets made of alloy AK-4 and connected thereto duralumin sheet. The stamped sheet has internal cavity to facilitate the weight of the wing. From the installation of the wing in the housing placed seven pins, which pass through the slot. The said channel input profile, raspolozhen¬ny on the engine and wing studs pass through slots curly profile.Wing.jpgWing

    Steering compartment is a metal housing made of aluminum alloy. The front and rear of the chassis has screw holes which connect the steering compartment with adjacent compartments (engine and tail fairing). Tail fairing consists of a hollow cylindrical fairing and proper sealing ring. The fairing pressed four nuts that are screwed in the screws that connect the steering compartment fairing. In front of the steering compartment at the bottom of the hatch is located, close lid, and employee access to a plug socket. The connector is mounted inside the housing on the bracket and is designed for electrical communication apparatus, placed inside the compartment with the missile units.
    Inside the compartment is placed the base, which establishes four pillars with bearings. It supports the axles are mounted earrings gas drives the rudders. At the rear of the base of four node detent wheel mounted and secured four legs. Each support is mounted on a ring attached bolt and serves for installation in her booster rocket. A lever connected through the shaft with the support, is connected via rollers (the puck) with a fork steering rod drive gas. Thus, any movement of the gas actuator stem (with razarretirovannom wheel) rotates the support and mounted on her wheel. The direction of the deviation of each of the four ru¬ley during ground inspections of functioning missile equipment is controlled by the inscriptions applied on the body compartment, front (on the fly) each support. Shafts arretirnym detent device consisting (for each shaft) of the piston and spring. Arretirnoe device is fixed with two screws. Moving the piston and out of the shaft groove occurs when entering the gas nozzle in the collector channel.
     The compartment is designed to control the aircraft during the flight, due to the supply of hot gas under pressure to the control units. Compartment consists of two main blocks: the collector and steering.Kinematics controls 2.jpgCompartment with rudders.jpgKinematics controls.jpg

    Compartment rudder control 2.jpgCompartment rudder controlCompartment rudder control 3.jpgCompartment rudder control 3

    Compartment rudder control 1_1.jpgCompartment rudder control

    The principle of operation of the collector compartment is as follows. As a result, the electric ignition pirosvechey mechanical discharger begins burning fuel charge in gas generators.
    Since the gas generators hot gas under high pressure, with filtration of fine and coarse particles is supplied to the charge collector, in which it is reduced from eight channels into one. The collector of the gas distributor, reducers, high and low pressure of the system supplying hot gases to the servos.compartment gas generators.jpgcompartment gas generators

    The aircraft air-to-air-September Winner

    Visionary

    My name is Denis, I am studying at the National Aerospace University "HAI", specialties of rocket and space complexes. This paper would like fashin the full range of course design. Your attention is available aircraft class "air-air". Rocket R-24 сompleted the normal aerodynamic scheme with destabilizers located on homing housing. The missile can be equipped with semi-active radar homing (R-24R) or heat (R-24T). The size and position destabilizers are selected depending on the type of GOS thus to maintain constant torque characteristics of a rocket.
    The most noticeable external difference between the new missiles on the P-23 was the use of forward-swept wings with the back edge. Changed and interior layout, the number of sections was reduced from 8 to 5. The first compartment has traditionally been a seeker. Rod warhead with a blast radius of 10 m and a slam-actuator is moved into the third compartment.Air-Air Missile 1.jpgAir-Air MissileAir-Air Missile.jpgAir-Air Missile 2

    Solid engine PRD-287 forms a fourth compartment. The engine has an increased work time, provides greater range and flight speed of up to M = 3.5. engine igniter.jpgengine igniterRocket engine solid fuel.jpgRocket engine solid fuel

    In the fifth compartment around the flue elongated nozzle unit housed gas generators providing power steering gears.The engine nozzle.jpgThe engine nozzle

    The wing has a trapezoidal form in plan and with sharpened edges of the front and rear sides. Linked wing body consists of extruded sheets made of alloy AK-4 and connected thereto duralumin sheet. The stamped sheet has internal cavity to facilitate the weight of the wing. From the installation of the wing in the housing placed seven pins, which pass through the slot. The said channel input profile, raspolozhen¬ny on the engine and wing studs pass through slots curly profile.Wing.jpgWing

    Steering compartment is a metal housing made of aluminum alloy. The front and rear of the chassis has screw holes which connect the steering compartment with adjacent compartments (engine and tail fairing). Tail fairing consists of a hollow cylindrical fairing and proper sealing ring. The fairing pressed four nuts that are screwed in the screws that connect the steering compartment fairing. In front of the steering compartment at the bottom of the hatch is located, close lid, and employee access to a plug socket. The connector is mounted inside the housing on the bracket and is designed for electrical communication apparatus, placed inside the compartment with the missile units.
    Inside the compartment is placed the base, which establishes four pillars with bearings. It supports the axles are mounted earrings gas drives the rudders. At the rear of the base of four node detent wheel mounted and secured four legs. Each support is mounted on a ring attached bolt and serves for installation in her booster rocket. A lever connected through the shaft with the support, is connected via rollers (the puck) with a fork steering rod drive gas. Thus, any movement of the gas actuator stem (with razarretirovannom wheel) rotates the support and mounted on her wheel. The direction of the deviation of each of the four ru¬ley during ground inspections of functioning missile equipment is controlled by the inscriptions applied on the body compartment, front (on the fly) each support. Shafts arretirnym detent device consisting (for each shaft) of the piston and spring. Arretirnoe device is fixed with two screws. Moving the piston and out of the shaft groove occurs when entering the gas nozzle in the collector channel.
     The compartment is designed to control the aircraft during the flight, due to the supply of hot gas under pressure to the control units. Compartment consists of two main blocks: the collector and steering.Kinematics controls 2.jpgCompartment with rudders.jpgKinematics controls.jpg

    Compartment rudder control 2.jpgCompartment rudder controlCompartment rudder control 3.jpgCompartment rudder control 3

    Compartment rudder control 1_1.jpgCompartment rudder control

    The principle of operation of the collector compartment is as follows. As a result, the electric ignition pirosvechey mechanical discharger begins burning fuel charge in gas generators.
    Since the gas generators hot gas under high pressure, with filtration of fine and coarse particles is supplied to the charge collector, in which it is reduced from eight channels into one. The collector of the gas distributor, reducers, high and low pressure of the system supplying hot gases to the servos.compartment gas generators.jpgcompartment gas generators

    • NX
  • I am Pranshu Dwivedi, designer of the AMIGO Vertical Axis Wind Turbine. I am a 4th year Aeronautical student at Inholland University of Applied Sciences, Delft -The Netherlands.

    The design represents a wind energy solution for urban green people, suitable design for cities to place at rooftops, backyards or gardens.

    The helical blade vertical axis wind turbine is designed using ANSYS. Most of the rotor structure is a combination of composite material with wood, which provided enough strength as well as a cool aesthetic look. The tower is made of Aluminium. At the bottom, the wooden box is present to hold everything together and damps the vibration issue in the structure as well.

    For more information, please feel free to contact

    Pranshu Dwivedi
    Contact no. (+31) 0633 055 806
    Email - pranshud@hotmail.com

    AMIGO Helical Blade Vertical Axis Wind Turbine

    Dreamer

    I am Pranshu Dwivedi, designer of the AMIGO Vertical Axis Wind Turbine. I am a 4th year Aeronautical student at Inholland University of Applied Sciences, Delft -The Netherlands.

    The design represents a wind energy solution for urban green people, suitable design for cities to place at rooftops, backyards or gardens.

    The helical blade vertical axis wind turbine is designed using ANSYS. Most of the rotor structure is a combination of composite material with wood, which provided enough strength as well as a cool aesthetic look. The tower is made of Aluminium. At the bottom, the wooden box is present to hold everything together and damps the vibration issue in the structure as well.

    For more information, please feel free to contact

    Pranshu Dwivedi
    Contact no. (+31) 0633 055 806
    Email - pranshud@hotmail.com

    • NX
  • University of Houston Industrial DesignCamera_Tripod_Final_01-Viewset 19.169.jpgCamera_Tripod_Final_01-Viewset 20.171.jpgCamera_Tripod_Final_01-Viewset 21.173.jpgCamera_Tripod_Final_01-Viewset 22.175.jpgCamera_Tripod_Final_01-Viewset 24.179.jpgCamera_Tripod_Final_01-Viewset 26.183.jpgCamera_Tripod_Final_01-Camera 15.152.jpgCamera_Tripod_Final_01-Camera 16.154.jpgCamera_Tripod_Final_01-Camera 19.158.jpgCamera_Tripod_Context_02B.jpgDesigned and modeled a DSLR camera and tripod using Siemens NX.  The final renders were done using Keyshot.  The concept behind this DSLR is a simple and minimialist dslr that only has the right amount of buttons so not to confuse users.  The tripod supplements this concept by having a simple tripod that is not overly complicated to setup.  The focus and appraoch was primarily on ergonomics and user-centered design.

    2017 November Winner - DSLR Camera and Tripod

    Enthusiast

    University of Houston Industrial DesignCamera_Tripod_Final_01-Viewset 19.169.jpgCamera_Tripod_Final_01-Viewset 20.171.jpgCamera_Tripod_Final_01-Viewset 21.173.jpgCamera_Tripod_Final_01-Viewset 22.175.jpgCamera_Tripod_Final_01-Viewset 24.179.jpgCamera_Tripod_Final_01-Viewset 26.183.jpgCamera_Tripod_Final_01-Camera 15.152.jpgCamera_Tripod_Final_01-Camera 16.154.jpgCamera_Tripod_Final_01-Camera 19.158.jpgCamera_Tripod_Context_02B.jpgDesigned and modeled a DSLR camera and tripod using Siemens NX.  The final renders were done using Keyshot.  The concept behind this DSLR is a simple and minimialist dslr that only has the right amount of buttons so not to confuse users.  The tripod supplements this concept by having a simple tripod that is not overly complicated to setup.  The focus and appraoch was primarily on ergonomics and user-centered design.

  • Portable speakers are everywhere nowadays, making them a must-have gadget. The variety of portable speakers are immense, with different approaches, being sound and style the most popular among companies. The portable speakers that have a gorgeous sound are hideous to look, in contrast with those that are appealing, that sound horrible. There was no speaker that possess both qualities until the A&H speaker was designed.

    The A&H portable speaker is a stunning piece of art. The A&H accomplish two of the most critical criteria for designing a portable speaker, sound and style. The A&H is a mono sound speaker, with a passive radiator to give the extra bass punch. The brain of the speaker is a powerful, but battery friendly amp, with Bluetooth capabilities and an aux output. The A&H have a gigantic battery that not only powers the unit itself, but it will let you change your phone. All this features are enclosed in the magnificent box with a leather and bronze finishing. The A&H portable speaker is the most beautiful speaker I ever seen, not because I design it, but because it is.

    I am a student at the University of Texas at Rio Grande Valley, and I design one of the most, if not the most, marvelous speaker of the market.

    Stylish Portable Speaker

    Theorist

    Portable speakers are everywhere nowadays, making them a must-have gadget. The variety of portable speakers are immense, with different approaches, being sound and style the most popular among companies. The portable speakers that have a gorgeous sound are hideous to look, in contrast with those that are appealing, that sound horrible. There was no speaker that possess both qualities until the A&H speaker was designed.

    The A&H portable speaker is a stunning piece of art. The A&H accomplish two of the most critical criteria for designing a portable speaker, sound and style. The A&H is a mono sound speaker, with a passive radiator to give the extra bass punch. The brain of the speaker is a powerful, but battery friendly amp, with Bluetooth capabilities and an aux output. The A&H have a gigantic battery that not only powers the unit itself, but it will let you change your phone. All this features are enclosed in the magnificent box with a leather and bronze finishing. The A&H portable speaker is the most beautiful speaker I ever seen, not because I design it, but because it is.

    I am a student at the University of Texas at Rio Grande Valley, and I design one of the most, if not the most, marvelous speaker of the market.

    • NX
  • One of my hobby is cycling, namely freeride. The pictures my first mountain bike, which was at one time dismantled and modeled on a computer. Now I switched to a new level of riding, and I now Rocky Mountain RMX.

    14_x_t.jpgMountain bike.34534534.jpgThe height of a bicycle with respect to human.34342342341.jpgCarbon steering wheel, and switches.

    Mountain bike

    Visionary

    One of my hobby is cycling, namely freeride. The pictures my first mountain bike, which was at one time dismantled and modeled on a computer. Now I switched to a new level of riding, and I now Rocky Mountain RMX.

    14_x_t.jpgMountain bike.34534534.jpgThe height of a bicycle with respect to human.34342342341.jpgCarbon steering wheel, and switches.

    • NX
  • Pokemon love has been all over the globe due to its 20 aniversary, Satoshi Tajiri its creator got this amaizing idea by looking back into his chilhood in Tokyo Japan. Mr. Tajiri was a bug catcher during its chilhood, so he practiced entomology as his pramary activity in a nearby forest in Machida, a western Tokyo suburb.
    The original idea was "Poket Monsters", but it was changed to a more appealing idea  "Pokemon"  due to its etymology. 

    Hi, my name is Samuel Molina, and my design is the Pokedex; "an electronic device designed to catalogue and provide information regarding the various species of Pokémon featured in the Pokémon video game, anime and manga series."This instrument will allow the player to know where pokemon are located in a specified region, types for each pokemon, and its description. 

    In specific, this "Pokedex" its from the "Pokemon" remake Omega Ruby and Alpha Sapphire from the original Ruby and Sapphire version. This design resembles a Game Boy Advance portatile console, pretty cool.


    It was desinged using Nx 10.0, for my Engineering design class at The University of Texas Rio Grande Valley. http://www.utrgv.edu/en-us/ 

     

     

    Pokedex: ORAS Remake Version

    Enthusiast

    Pokemon love has been all over the globe due to its 20 aniversary, Satoshi Tajiri its creator got this amaizing idea by looking back into his chilhood in Tokyo Japan. Mr. Tajiri was a bug catcher during its chilhood, so he practiced entomology as his pramary activity in a nearby forest in Machida, a western Tokyo suburb.
    The original idea was "Poket Monsters", but it was changed to a more appealing idea  "Pokemon"  due to its etymology. 

    Hi, my name is Samuel Molina, and my design is the Pokedex; "an electronic device designed to catalogue and provide information regarding the various species of Pokémon featured in the Pokémon video game, anime and manga series."This instrument will allow the player to know where pokemon are located in a specified region, types for each pokemon, and its description. 

    In specific, this "Pokedex" its from the "Pokemon" remake Omega Ruby and Alpha Sapphire from the original Ruby and Sapphire version. This design resembles a Game Boy Advance portatile console, pretty cool.


    It was desinged using Nx 10.0, for my Engineering design class at The University of Texas Rio Grande Valley. http://www.utrgv.edu/en-us/ 

     

     

    • NX